Team,
is there a dependency between enabling the WIFI part and the BT part?
My customer gets a hciattach timeout each second time when trying to enable BT when WIFI is already enabled.
The issues does not occur when WIFI is deactivated.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
is there a dependency between enabling the WIFI part and the BT part?
My customer gets a hciattach timeout each second time when trying to enable BT when WIFI is already enabled.
The issues does not occur when WIFI is deactivated.
Thanks
Franziskus,
Please try the following steps when using hciattach to enable Bluetooth controller. (Note : # below represents the gpio number that is connected to the BT_EN pin and $ represents the tty port connected to HCI pins)
echo # > /sys/class/gpio/export echo "out" > /sys/class/gpio/gpio#/direction echo 0 > /sys/class/gpio/gpio#/value echo 1 > /sys/class/gpio/gpio#/value echo 0 > /sys/class/gpio/gpio#/value echo 1 > /sys/class/gpio/gpio#/value hciattach /dev/tty$ texas 3000000
This will result in two low to high transitions of BT_EN signal each time hciattach is called. Please see if this resolves the issue.
Best regards,
Vihang