Part Number: CC3100MODBOOST
I'm using the CC3100MODBOOST board in AP mode attached to another board for development.
After entering AP mode, stopping, configurting, and starting DHCP, I connect with a windows laptop and am unable to get a IP address from the CC3100's DHCP server. It doesn't appear to be answering DHCP DISCOVER messages. As of yet, I haven't gotten it to work with any devices.
CC3100 FW and driver versions:
ID(67108864) FW(31.1.5.0.2) PHY(1.0.3.37)
NWP(2.11.0.1) ROM(13107) HostDrv(1.0.1.11)
Static AP settings:
AP IP: 192.168.1.1
AP Gateway: 192.168.1.1
AP DNS: 192.168.1.1
AP Mask: 255.255.255.0
DHCP Server settings:
DHCP Lease Time: 4096 ms
DHCP IP Start: 192.168.1.2
DHCP IP End: 192.168.1.11
NWP log attached:
Wireshark log attached for the same time period: