Other Parts Discussed in Thread: CC3120, SYSCONFIG
Hello,
Regarding this page in the "Academy"
Specifically steps 3 and 4.
Step 3: I entered my local WiFi settings. However the device is STILL in AP mode and my tablet remains connected to it...
Step 4: says to ping... I can tell it to ping itself, and that works find. But part 3 says ping the connected device by looking under the "Station" tab. Well the "Station" TAB only has my MAC address listed.
However, under the STATUS tab, Stations SECTION, it does show an IP address. It tells me the station is 192.168.1.101
And another HOWEVER, this IP address is NOT what was assigned to my device.
The CC3120 is 10.123.45.1 and it assigned my tablet 10.123.45.2 I can ping that just fine.
Then in part 4, it tells me to ping the google address. Seriously...? With no gateway connected to the device, it will never be able to reach outside this subnet.
So...
Where is this 192.168.1.101 that it claims was assigned coming from??
Was I supposed to change the device to Station mode in step 3? That's the only way to ping outside of it's subnet... Obviously once I do that, my tablet will be disconnected, as that SSID is gone.
So I changed the device to station mode using the web page, now it connects to my network, under IP 192.168.1.91. I had to hunt that down on my router.... So now to connect I had to know how to find it, and connect to it from from a device that is on my network.