This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF: CC3220sf is not going to LPDS mode using (TIDC-01005) wifi door lock reference design

Part Number: CC3220SF
Other Parts Discussed in Thread: TIDC-01005, CC3220S, UNIFLASH

Hello,

I am working on CC3220sf and building my application on TIDC-01005  WIFI door lock reference  design software.

As we are in a stage we need to check for the power consumption of our custom board we are observing the CC3220sf is not going to LPDS(Low power deep sleep) mode.

As i have built my application on TIDC-01005 software i have not changed any of the basic timeouts like LSI (Long Sleep Interval) which is still 500ms.

In the document TI Designs: TIDC-01005 Battery-Powered, Smart-Lock Reference Design With Cloud Connectivity Using SimpleLink™ Wi-Fi  section

2.4.9 Low-Power Consumption it is mentioned as below

TI-Drivers include a power manager that puts the MCU subsystem of the CC3220S into low-power modes when the system is idle. In the TIDC-01005, the MCU enters LPDS any time the idle task is executed. The network processor subsystem of the CC3220S uses a policy called Long Sleep Interval (LSI) to increase the amount of time the Wi-Fi NWP spends in a low-power mode between AP beacons and broadcasts, which can significantly reduce the average power consumption. The maximum sleep interval allowed by default in the TIDC-01005 software is 500 milliseconds, but the actual amount of time the Wi-Fi NWP spends in LPDS depends on the parameters of the AP (for example, beacon interval and DTIM value). 

In above paragraph i didn't get the point saying actual amount of time the Wi-Fi NWP spends in LPDS depends on the parameters of the AP (for example, beacon interval and DTIM value).

What is beacon interval and DMIT value? Is it mentioned anywhere in the software? 

Regards,

Sanath Rai

  • Hi Sanath,

    The purpose of that sentence is to point out that the behavior of the AP the CC3220 is connected to will affect its power consumption. The parameters mentioned, the beacon interval and DTIM value concern how often the AP will send out beacons with the DTIM bit set, i.e. how often the CC3220 will need to wake up if it doesn't want to potentially miss multicast data delivered in those DTIMs.

    The wiki page has some info: https://en.wikipedia.org/wiki/Delivery_traffic_indication_message

    A deep technical explanation of 802.11 power save, including the impact of the DTIM on the various power save modes can be found here: https://dot11zen.blogspot.com/2018/02/80211-power-management-with-packet.html

    Since the DTIM and beacon interval settings are set at the AP and cannot be controlled by the AP, it is simply something that you will need to keep in mind when performing power measurement.

    Let me know if you need more clarification or have further questions.

    Regards,

    Michael

  • Hi Michael,

    Thanks for the detailed information.

    So according to this i need to change the flow of my code or else it will not work out because our board is not entering LPDS mode.its taking upto 20 mA continuously which means its engaging in some activity as you explained.

    As our application is based on battery operation power consumption is main factor.

    Any suggestions from your side on how to deal with this?

    Regards,

    Sanath Rai

  • HI Sanath,

    Have you defined the USE_POWER_POLICY symbol? As explained in the design guide, by default LPDS is actually turned off, in order to allow you to use the debugger with the wifi_doorlock design. You'll need to add that to your predefined symbols in your compiler to get LPDS working if you haven't already. Please do so and recheck the power consumption.

    Regards,

    Michael

  • Hi Michael,

    Thank you for the point you suggested.

    That was a mistake from my side i had not seen that section in the document.I have added the USE_POWER_POLICY predefined symbol and have built the code and dumped it via UNIFLASH. 

    i just checked it after the changes made still its showing the same current consumption(20mA) .As per document it should show around 377 micro Amps.

    i feel its still not entering LPDS.

    Any further changes need to be done other than that?

    i will just brief you our application.

    All the basic things i have built on wifi door lock reference design like MQTT ,we are not using Bluetooth,OTA,motor and the sensors so i have disabled them.

    i have added one more Button interrupt for our application along with the existing button interrupt.

    one more point is the original wifi door lock reference design is built for cc3220s ,right now i am using cc3220sf. I have built the code for CC3220sf using CCS and Functionality wise our custom board with cc3220sf  is working fine without any issues. Only issue we are facing is that its not entering LPDS and consuming 20mA.

    Anything Hardware changes need to be done? and is there any way to check whether its going to LPDS or not?

    i will attach the configuration file for your reference.

    /*
     * Copyright (c) 2016-2017, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== CC3220S_LAUNCHXL.c ========
     *  This file is responsible for setting up the board specific items for the
     *  CC3220S_LAUNCHXL board.
     */
    
    #include <stdbool.h>
    #include <stddef.h>
    #include <stdint.h>
    
    #include <ti/devices/cc32xx/inc/hw_ints.h>
    #include <ti/devices/cc32xx/inc/hw_memmap.h>
    #include <ti/devices/cc32xx/inc/hw_types.h>
    
    #include <ti/devices/cc32xx/driverlib/rom.h>
    #include <ti/devices/cc32xx/driverlib/rom_map.h>
    #include <ti/devices/cc32xx/driverlib/adc.h>
    #include <ti/devices/cc32xx/driverlib/gpio.h>
    #include <ti/devices/cc32xx/driverlib/pin.h>
    #include <ti/devices/cc32xx/driverlib/prcm.h>
    #include <ti/devices/cc32xx/driverlib/spi.h>
    #include <ti/devices/cc32xx/driverlib/sdhost.h>
    #include <ti/devices/cc32xx/driverlib/timer.h>
    #include <ti/devices/cc32xx/driverlib/uart.h>
    #include <ti/devices/cc32xx/driverlib/udma.h>
    #include <ti/devices/cc32xx/driverlib/wdt.h>
    
    #include <ti/drivers/Power.h>
    #include <ti/drivers/power/PowerCC32XX.h>
    
    #include "CC3220S_LAUNCHXL.h"
    
    /*
     *  This define determines whether to use the UARTCC32XXDMA driver
     *  or the UARTCC32XX (no DMA) driver.  Set to 1 to use the UARTCC32XXDMA
     *  driver.
     */
    #ifndef TI_DRIVERS_UART_DMA
    #define TI_DRIVERS_UART_DMA 0
    #endif
    
    /*
     *  =============================== ADC ===============================
     */
    #include <ti/drivers/ADC.h>
    #include <ti/drivers/adc/ADCCC32XX.h>
    
    ADCCC32XX_Object adcCC3220SObjects[CC3220S_LAUNCHXL_ADCCOUNT];
    
    const ADCCC32XX_HWAttrsV1 adcCC3220SHWAttrs[CC3220S_LAUNCHXL_ADCCOUNT] = {
        {
            .adcPin = ADCCC32XX_PIN_59_CH_2
        },
        {
            .adcPin = ADCCC32XX_PIN_60_CH_3
        }
    };
    
    const ADC_Config ADC_config[CC3220S_LAUNCHXL_ADCCOUNT] = {
        {
            .fxnTablePtr = &ADCCC32XX_fxnTable,
            .object = &adcCC3220SObjects[CC3220S_LAUNCHXL_ADC0],
            .hwAttrs = &adcCC3220SHWAttrs[CC3220S_LAUNCHXL_ADC0]
        },
        {
            .fxnTablePtr = &ADCCC32XX_fxnTable,
            .object = &adcCC3220SObjects[CC3220S_LAUNCHXL_ADC1],
            .hwAttrs = &adcCC3220SHWAttrs[CC3220S_LAUNCHXL_ADC1]
        }
    };
    
    const uint_least8_t ADC_count = CC3220S_LAUNCHXL_ADCCOUNT;
    
    /*
     *  =============================== Capture ===============================
     */
    #include <ti/drivers/Capture.h>
    #include <ti/drivers/capture/CaptureCC32XX.h>
    
    CaptureCC32XX_Object captureCC3220SObjects[CC3220S_LAUNCHXL_CAPTURECOUNT];
    
    const CaptureCC32XX_HWAttrs captureCC3220SHWAttrs[CC3220S_LAUNCHXL_CAPTURECOUNT] =
    {
          {
             .capturePin = CaptureCC32XX_PIN_04,
             .intPriority = ~0
          },
          {
              .capturePin = CaptureCC32XX_PIN_05,
              .intPriority = ~0
          },
    };
    
    const Capture_Config Capture_config[CC3220S_LAUNCHXL_CAPTURECOUNT] = {
        {
            .fxnTablePtr = &CaptureCC32XX_fxnTable,
            .object = &captureCC3220SObjects[CC3220S_LAUNCHXL_CAPTURE0],
            .hwAttrs = &captureCC3220SHWAttrs[CC3220S_LAUNCHXL_CAPTURE0]
        },
        {
            .fxnTablePtr = &CaptureCC32XX_fxnTable,
            .object = &captureCC3220SObjects[CC3220S_LAUNCHXL_CAPTURE1],
            .hwAttrs = &captureCC3220SHWAttrs[CC3220S_LAUNCHXL_CAPTURE1]
        }
    };
    
    const uint_least8_t Capture_count = CC3220S_LAUNCHXL_CAPTURECOUNT;
    
    /*
     *  =============================== Crypto ===============================
     */
    #include <ti/drivers/crypto/CryptoCC32XX.h>
    
    CryptoCC32XX_Object cryptoCC3220SObjects[CC3220S_LAUNCHXL_CRYPTOCOUNT];
    
    const CryptoCC32XX_Config CryptoCC32XX_config[CC3220S_LAUNCHXL_CRYPTOCOUNT] = {
        {
            .object = &cryptoCC3220SObjects[CC3220S_LAUNCHXL_CRYPTO0]
        }
    };
    
    const uint_least8_t CryptoCC32XX_count = CC3220S_LAUNCHXL_CRYPTOCOUNT;
    
    /*
     *  =============================== DMA ===============================
     */
    #include <ti/drivers/dma/UDMACC32XX.h>
    
    #if defined(__TI_COMPILER_VERSION__)
    #pragma DATA_ALIGN(dmaControlTable, 1024)
    #elif defined(__IAR_SYSTEMS_ICC__)
    #pragma data_alignment=1024
    #elif defined(__GNUC__)
    __attribute__ ((aligned (1024)))
    #endif
    static tDMAControlTable dmaControlTable[64];
    
    /*
     *  ======== dmaErrorFxn ========
     *  This is the handler for the uDMA error interrupt.
     */
    static void dmaErrorFxn(uintptr_t arg)
    {
        int status = MAP_uDMAErrorStatusGet();
        MAP_uDMAErrorStatusClear();
    
        /* Suppress unused variable warning */
        (void)status;
    
        while (1);
    }
    
    UDMACC32XX_Object udmaCC3220SObject;
    
    const UDMACC32XX_HWAttrs udmaCC3220SHWAttrs = {
        .controlBaseAddr = (void *)dmaControlTable,
        .dmaErrorFxn = (UDMACC32XX_ErrorFxn)dmaErrorFxn,
        .intNum = INT_UDMAERR,
        .intPriority = (~0)
    };
    
    const UDMACC32XX_Config UDMACC32XX_config = {
        .object = &udmaCC3220SObject,
        .hwAttrs = &udmaCC3220SHWAttrs
    };
    
    /*
     *  =============================== General ===============================
     */
    /*
     *  ======== CC3220S_LAUNCHXL_initGeneral ========
     */
    void CC3220S_LAUNCHXL_initGeneral(void)
    {
        PRCMCC3200MCUInit();
        Power_init();
    }
    
    /*
     *  =============================== GPIO ===============================
     */
    #include <ti/drivers/GPIO.h>
    #include <ti/drivers/gpio/GPIOCC32XX.h>
    
    /*
     * Array of Pin configurations
     * NOTE: The order of the pin configurations must coincide with what was
     *       defined in CC3220S_LAUNCHXL.h
     * NOTE: Pins not used for interrupts should be placed at the end of the
     *       array.  Callback entries can be omitted from callbacks array to
     *       reduce memory usage.
     */
    GPIO_PinConfig gpioPinConfigs[] = {
        /* input pins with callbacks */
        /* CC3220S_LAUNCHXL_GPIO_SW3 */
        GPIOCC32XX_GPIO_22 | GPIO_CFG_INPUT | GPIO_CFG_IN_PD | GPIO_CFG_IN_INT_BOTH_EDGES,
        GPIOCC32XX_GPIO_13 | GPIO_CFG_INPUT | GPIO_CFG_IN_PD | GPIO_CFG_IN_INT_BOTH_EDGES,
    
        /* output pins */
        /* CC3220S_LAUNCHXL_GPIO_LED_D7 */
        GPIOCC32XX_GPIO_09 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
    
        /*
         *  CC3220S_LAUNCHXL_GPIO_LED_D5 and CC3220S_LAUNCHXL_GPIO_LED_D6 are shared with the
         *  I2C and PWM peripherals. In order for those examples to work, these
         *  LEDs are taken out of gpioPinConfig[]
         */
        /* CC3220S_LAUNCHXL_GPIO_LED_D6 */
        GPIOCC32XX_GPIO_10 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
        /* CC3220S_LAUNCHXL_GPIO_LED_D5 */
        GPIOCC32XX_GPIO_11 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
    
        /* CC3220S_LAUNCHXL_GPIO_P16 (Motor Driver IN1) */
        GPIOCC32XX_GPIO_23 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
        /* CC3220S_LAUNCHXL_GPIO_P18 (Motor Driver nSleep) */
        GPIOCC32XX_GPIO_28 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
    
        /*
         * Pins needed to support power management with the NPI to BLE device and BMI sensor
         */
    
        /* CC3220S_LAUNCHXL_IN1 for BMI160 */
        GPIOCC32XX_GPIO_06 | GPIO_CFG_IN_PD | GPIO_CFG_IN_INT_RISING,
    
        /* CC3220S_LAUNCHXL_RESET */
        GPIOCC32XX_GPIO_16 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_HIGH,
    
        /* CC3220S_LAUNCHXL_MRDY */
        GPIOCC32XX_GPIO_07 | GPIO_CFG_IN_PU,
    
        /* CC3220S_LAUNCHXL_SRDY */
        GPIOCC32XX_GPIO_17 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_HIGH,
    };
    
    /*
     * Array of callback function pointers
     * NOTE: The order of the pin configurations must coincide with what was
     *       defined in CC3220S_LAUNCHXL.h
     * NOTE: Pins not used for interrupts can be omitted from callbacks array to
     *       reduce memory usage (if placed at end of gpioPinConfigs array).
     */
    GPIO_CallbackFxn gpioCallbackFunctions[] = {
        NULL,  /* CC3220S_LAUNCHXL_GPIO_SW3 */
        NULL,  /* CC3220S_LAUNCHXL_GPIO_SW2 */
        NULL   /* CC3220S_MRDY */
    };
    
    /* The device-specific GPIO_config structure */
    const GPIOCC32XX_Config GPIOCC32XX_config = {
        .pinConfigs = (GPIO_PinConfig *)gpioPinConfigs,
        .callbacks = (GPIO_CallbackFxn *)gpioCallbackFunctions,
        .numberOfPinConfigs = sizeof(gpioPinConfigs)/sizeof(GPIO_PinConfig),
        .numberOfCallbacks = sizeof(gpioCallbackFunctions)/sizeof(GPIO_CallbackFxn),
        .intPriority = (~0)
    };
    
    ///*
    // *  ============================= Display =============================
    // */
    #include <ti/display/Display.h>
    #include <ti/display/DisplayUart.h>
    #define MAXPRINTLEN 768
    
    DisplayUart_Object displayUartObject;
    
    static char displayBuf[MAXPRINTLEN];
    
    const DisplayUart_HWAttrs displayUartHWAttrs = {
        .uartIdx = 1,
        .baudRate = 115200,
        .mutexTimeout = (unsigned int)(-1),
        .strBuf = displayBuf,
        .strBufLen = MAXPRINTLEN
    };
    
    #ifndef BOARD_DISPLAY_USE_UART_ANSI
    #define BOARD_DISPLAY_USE_UART_ANSI 0
    #endif
    
    const Display_Config Display_config[] = {
        {
    #  if (BOARD_DISPLAY_USE_UART_ANSI)
            .fxnTablePtr = &DisplayUartAnsi_fxnTable,
    #  else /* Default to minimal UART with no cursor placement */
            .fxnTablePtr = &DisplayUartMin_fxnTable,
    #  endif
            .object = &displayUartObject,
            .hwAttrs = &displayUartHWAttrs
        }
    };
    
    const uint_least8_t Display_count = sizeof(Display_config) / sizeof(Display_Config);
    
    /*
     *  =============================== I2C ===============================
     */
    #include <ti/drivers/I2C.h>
    #include <ti/drivers/i2c/I2CCC32XX.h>
    
    I2CCC32XX_Object i2cCC3220SObjects[CC3220S_LAUNCHXL_I2CCOUNT];
    
    const I2CCC32XX_HWAttrsV1 i2cCC3220SHWAttrs[CC3220S_LAUNCHXL_I2CCOUNT] = {
        {
            .baseAddr = I2CA0_BASE,
            .intNum = INT_I2CA0,
            .intPriority = (~0),
            .clkPin = I2CCC32XX_PIN_01_I2C_SCL,
            .dataPin = I2CCC32XX_PIN_02_I2C_SDA
        }
    };
    
    const I2C_Config I2C_config[CC3220S_LAUNCHXL_I2CCOUNT] = {
        {
            .fxnTablePtr = &I2CCC32XX_fxnTable,
            .object = &i2cCC3220SObjects[CC3220S_LAUNCHXL_I2C0],
            .hwAttrs = &i2cCC3220SHWAttrs[CC3220S_LAUNCHXL_I2C0]
        }
    };
    
    const uint_least8_t I2C_count = CC3220S_LAUNCHXL_I2CCOUNT;
    
    /*
     *  =============================== I2S ===============================
     */
    #include <ti/drivers/I2S.h>
    //#include <ti/drivers/i2s/I2SCC32XXDMA.h>
    
    //I2SCC32XXDMA_Object i2sCC3220SObjects[CC3220S_LAUNCHXL_I2SCOUNT];
    //
    //const I2SCC32XXDMA_HWAttrsV1 i2sCC3220SHWAttrs[CC3220S_LAUNCHXL_I2SCOUNT] = {
    //    {
    //        .baseAddr = I2S_BASE,
    //        .intNum = INT_I2S,
    //        .intPriority = (~0),
    //        .rxChannelIndex = UDMA_CH4_I2S_RX,
    //        .txChannelIndex = UDMA_CH5_I2S_TX,
    //        .xr0Pin = I2SCC32XXDMA_PIN_64_McAXR0,
    //        .xr1Pin = I2SCC32XXDMA_PIN_50_McAXR1,
    //        .clkxPin = I2SCC32XXDMA_PIN_62_McACLKX,
    //        .clkPin = I2SCC32XXDMA_PIN_53_McACLK,
    //        .fsxPin = I2SCC32XXDMA_PIN_63_McAFSX,
    //    }
    //};
    //
    //const I2S_Config I2S_config[CC3220S_LAUNCHXL_I2SCOUNT] = {
    //    {
    //        .fxnTablePtr = &I2SCC32XXDMA_fxnTable,
    //        .object = &i2sCC3220SObjects[CC3220S_LAUNCHXL_I2S0],
    //        .hwAttrs = &i2sCC3220SHWAttrs[CC3220S_LAUNCHXL_I2S0]
    //    }
    //};
    //
    //const uint_least8_t I2S_count = CC3220S_LAUNCHXL_I2SCOUNT;
    
    /*
     *  =============================== Power ===============================
     */
    /*
     * This table defines the parking state to be set for each parkable pin
     * during LPDS. (Device pins must be parked during LPDS to achieve maximum
     * power savings.)  If the pin should be left unparked, specify the state
     * PowerCC32XX_DONT_PARK.  For example, for a UART TX pin, the device
     * will automatically park the pin in a high state during transition to LPDS,
     * so the Power Manager does not need to explictly park the pin.  So the
     * corresponding entries in this table should indicate PowerCC32XX_DONT_PARK.
     */
    PowerCC32XX_ParkInfo parkInfo[] = {
    /*          PIN                    PARK STATE              PIN ALIAS (FUNCTION)
         -----------------  ------------------------------     -------------------- */
        {PowerCC32XX_PIN01, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO10              */
        {PowerCC32XX_PIN02, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO11              */
        {PowerCC32XX_PIN03, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO12              */
        {PowerCC32XX_PIN04, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO13              */
        {PowerCC32XX_PIN05, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO14              */
        {PowerCC32XX_PIN06, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO15              */
        {PowerCC32XX_PIN07, PowerCC32XX_WEAK_PULL_UP_STD}, /* GPIO16              */
        {PowerCC32XX_PIN08, PowerCC32XX_WEAK_PULL_UP_STD}, /* GPIO17              */
        {PowerCC32XX_PIN13, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* FLASH_SPI_DIN       */
        {PowerCC32XX_PIN15, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO22              */
        {PowerCC32XX_PIN16, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* TDI (JTAG DEBUG)    */
        {PowerCC32XX_PIN17, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* TDO (JTAG DEBUG)    */
        {PowerCC32XX_PIN19, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* TCK (JTAG DEBUG)    */
        {PowerCC32XX_PIN20, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* TMS (JTAG DEBUG)    */
        {PowerCC32XX_PIN18, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO28              */
        {PowerCC32XX_PIN21, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* SOP2                */
        {PowerCC32XX_PIN29, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* ANTSEL1             */
        {PowerCC32XX_PIN30, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* ANTSEL2             */
        {PowerCC32XX_PIN45, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* DCDC_ANA2_SW_P      */
        {PowerCC32XX_PIN50, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO0               */
        {PowerCC32XX_PIN52, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* RTC_XTAL_N          */
        {PowerCC32XX_PIN53, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO30              */
        {PowerCC32XX_PIN55, PowerCC32XX_WEAK_PULL_UP_STD},   /* GPIO1 (XDS_UART_RX) */
        {PowerCC32XX_PIN57, PowerCC32XX_WEAK_PULL_UP_STD},   /* GPIO2 (XDS_UART_TX) */
        {PowerCC32XX_PIN58, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO3               */
        {PowerCC32XX_PIN59, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO4               */
        {PowerCC32XX_PIN60, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO5               */
        {PowerCC32XX_PIN61, PowerCC32XX_WEAK_PULL_UP_STD}, /* GPIO6               */
        {PowerCC32XX_PIN62, PowerCC32XX_WEAK_PULL_UP_STD}, /* GPIO7               */
        {PowerCC32XX_PIN63, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO8               */
        {PowerCC32XX_PIN64, PowerCC32XX_WEAK_PULL_DOWN_STD}, /* GPIO9               */
    };
    
    /*
     *  This structure defines the configuration for the Power Manager.
     *
     *  In this configuration the Power policy is disabled by default (because
     *  enablePolicy is set to false).  The Power policy can be enabled dynamically
     *  at runtime by calling Power_enablePolicy(), or at build time, by changing
     *  enablePolicy to true in this structure.
     */
    const PowerCC32XX_ConfigV1 PowerCC32XX_config = {
        .policyInitFxn = &PowerCC32XX_initPolicy,
        .policyFxn = &PowerCC32XX_sleepPolicy,
        .enterLPDSHookFxn = NULL,
        .resumeLPDSHookFxn = NULL,
        .enablePolicy = true,
        .enableGPIOWakeupLPDS = true,
        .enableGPIOWakeupShutdown = true,
        .enableNetworkWakeupLPDS = true,
        .wakeupGPIOSourceLPDS = PRCM_LPDS_GPIO13,
        .wakeupGPIOTypeLPDS = PRCM_LPDS_RISE_EDGE,
        .wakeupGPIOFxnLPDS = NULL,
        .wakeupGPIOFxnLPDSArg = 0,
        .wakeupGPIOSourceShutdown = PRCM_HIB_GPIO13,
        .wakeupGPIOTypeShutdown = PRCM_HIB_RISE_EDGE,
        .ramRetentionMaskLPDS = PRCM_SRAM_COL_1 | PRCM_SRAM_COL_2 |
            PRCM_SRAM_COL_3 | PRCM_SRAM_COL_4,
        .keepDebugActiveDuringLPDS = false,
        .ioRetentionShutdown = PRCM_IO_RET_GRP_1,
        .pinParkDefs = parkInfo,
        .numPins = sizeof(parkInfo) / sizeof(PowerCC32XX_ParkInfo)
    };
    
    /*
     *  =============================== PWM ===============================
     */
    #include <ti/drivers/PWM.h>
    #include <ti/drivers/pwm/PWMTimerCC32XX.h>
    
    PWMTimerCC32XX_Object pwmTimerCC3220SObjects[CC3220S_LAUNCHXL_PWMCOUNT];
    
    const PWMTimerCC32XX_HWAttrsV2 pwmTimerCC3220SHWAttrs[CC3220S_LAUNCHXL_PWMCOUNT] = {
        {    /* CC3220S_LAUNCHXL_PWM6 */
            .pwmPin = PWMTimerCC32XX_PIN_17
        },
    };
    
    const PWM_Config PWM_config[CC3220S_LAUNCHXL_PWMCOUNT] = {
        {
            .fxnTablePtr = &PWMTimerCC32XX_fxnTable,
            .object = &pwmTimerCC3220SObjects[CC3220S_LAUNCHXL_PWM0],
            .hwAttrs = &pwmTimerCC3220SHWAttrs[CC3220S_LAUNCHXL_PWM0]
        },
    };
    
    const uint_least8_t PWM_count = CC3220S_LAUNCHXL_PWMCOUNT;
    
    /*
     *  =============================== SDFatFS ===============================
     */
    #include <ti/drivers/SD.h>
    #include <ti/drivers/SDFatFS.h>
    
    /*
     * Note: The SDFatFS driver provides interface functions to enable FatFs
     * but relies on the SD driver to communicate with SD cards.  Opening a
     * SDFatFs driver instance will internally try to open a SD driver instance
     * reusing the same index number (opening SDFatFs driver at index 0 will try to
     * open SD driver at index 0).  This requires that all SDFatFs driver instances
     * have an accompanying SD driver instance defined with the same index.  It is
     * acceptable to have more SD driver instances than SDFatFs driver instances
     * but the opposite is not supported & the SDFatFs will fail to open.
     */
    SDFatFS_Object sdfatfsObjects[CC3220S_LAUNCHXL_SDFatFSCOUNT];
    
    const SDFatFS_Config SDFatFS_config[CC3220S_LAUNCHXL_SDFatFSCOUNT] = {
        {
            .object = &sdfatfsObjects[CC3220S_LAUNCHXL_SDFatFS0]
        }
    };
    
    const uint_least8_t SDFatFS_count = CC3220S_LAUNCHXL_SDFatFSCOUNT;
    
    /*
     *  =============================== SD ===============================
     */
    #include <ti/drivers/SD.h>
    #include <ti/drivers/sd/SDHostCC32XX.h>
    
    SDHostCC32XX_Object sdhostCC3220SObjects[CC3220S_LAUNCHXL_SDCOUNT];
    
    /* SDHost configuration structure, describing which pins are to be used */
    const SDHostCC32XX_HWAttrsV1 sdhostCC3220SHWattrs[CC3220S_LAUNCHXL_SDCOUNT] = {
        {
            .clkRate = 8000000,
            .intPriority = ~0,
            .baseAddr = SDHOST_BASE,
            .rxChIdx = UDMA_CH23_SDHOST_RX,
            .txChIdx = UDMA_CH24_SDHOST_TX,
            .dataPin = SDHostCC32XX_PIN_06_SDCARD_DATA,
            .cmdPin = SDHostCC32XX_PIN_08_SDCARD_CMD,
            .clkPin = SDHostCC32XX_PIN_07_SDCARD_CLK
        }
    };
    
    const SD_Config SD_config[CC3220S_LAUNCHXL_SDCOUNT] = {
        {
            .fxnTablePtr = &sdHostCC32XX_fxnTable,
            .object = &sdhostCC3220SObjects[CC3220S_LAUNCHXL_SD0],
            .hwAttrs = &sdhostCC3220SHWattrs[CC3220S_LAUNCHXL_SD0]
        },
    };
    
    const uint_least8_t SD_count = CC3220S_LAUNCHXL_SDCOUNT;
    
    /*
     *  =============================== SPI ===============================
     */
    #include <ti/drivers/SPI.h>
    #include <ti/drivers/spi/SPICC32XXDMA.h>
    
    SPICC32XXDMA_Object spiCC3220SDMAObjects[CC3220S_LAUNCHXL_SPICOUNT];
    
    #if defined(__TI_COMPILER_VERSION__)
    #pragma DATA_ALIGN(spiCC3220SDMAscratchBuf, 32)
    #elif defined(__IAR_SYSTEMS_ICC__)
    #pragma data_alignment=32
    #elif defined(__GNUC__)
    __attribute__ ((aligned (32)))
    #endif
    uint32_t spiCC3220SDMAscratchBuf[CC3220S_LAUNCHXL_SPICOUNT];
    
    const SPICC32XXDMA_HWAttrsV1 spiCC3220SDMAHWAttrs[CC3220S_LAUNCHXL_SPICOUNT] = {
        /* index 0 is reserved for LSPI that links to the NWP */
        {
            .baseAddr = LSPI_BASE,
            .intNum = INT_LSPI,
            .intPriority = (~0),
            .spiPRCM = PRCM_LSPI,
            .csControl = SPI_SW_CTRL_CS,
            .csPolarity = SPI_CS_ACTIVEHIGH,
            .pinMode = SPI_4PIN_MODE,
            .turboMode = SPI_TURBO_OFF,
            .scratchBufPtr = &spiCC3220SDMAscratchBuf[CC3220S_LAUNCHXL_SPI0],
            .defaultTxBufValue = 0,
            .rxChannelIndex = UDMA_CH12_LSPI_RX,
            .txChannelIndex = UDMA_CH13_LSPI_TX,
            .minDmaTransferSize = 100,
            .mosiPin = SPICC32XXDMA_PIN_NO_CONFIG,
            .misoPin = SPICC32XXDMA_PIN_NO_CONFIG,
            .clkPin = SPICC32XXDMA_PIN_NO_CONFIG,
            .csPin = SPICC32XXDMA_PIN_NO_CONFIG
        },
        {
            .baseAddr = GSPI_BASE,
            .intNum = INT_GSPI,
            .intPriority = (~0),
            .spiPRCM = PRCM_GSPI,
            .csControl = SPI_HW_CTRL_CS,
            .csPolarity = SPI_CS_ACTIVELOW,
            .pinMode = SPI_4PIN_MODE,
            .turboMode = SPI_TURBO_OFF,
            .scratchBufPtr = &spiCC3220SDMAscratchBuf[CC3220S_LAUNCHXL_SPI1],
            .defaultTxBufValue = 0,
            .rxChannelIndex = UDMA_CH6_GSPI_RX,
            .txChannelIndex = UDMA_CH7_GSPI_TX,
            .minDmaTransferSize = 100,
            .mosiPin = SPICC32XXDMA_PIN_07_MOSI,
            .misoPin = SPICC32XXDMA_PIN_06_MISO,
            .clkPin = SPICC32XXDMA_PIN_05_CLK,
            .csPin = SPICC32XXDMA_PIN_08_CS
        }
    };
    
    const SPI_Config SPI_config[CC3220S_LAUNCHXL_SPICOUNT] = {
        {
            .fxnTablePtr = &SPICC32XXDMA_fxnTable,
            .object = &spiCC3220SDMAObjects[CC3220S_LAUNCHXL_SPI0],
            .hwAttrs = &spiCC3220SDMAHWAttrs[CC3220S_LAUNCHXL_SPI0]
        },
        {
            .fxnTablePtr = &SPICC32XXDMA_fxnTable,
            .object = &spiCC3220SDMAObjects[CC3220S_LAUNCHXL_SPI1],
            .hwAttrs = &spiCC3220SDMAHWAttrs[CC3220S_LAUNCHXL_SPI1]
        }
    };
    
    const uint_least8_t SPI_count = CC3220S_LAUNCHXL_SPICOUNT;
    
    /*
     *  =============================== Timer ===============================
     */
    #include <ti/drivers/Timer.h>
    #include <ti/drivers/timer/TimerCC32XX.h>
    
    TimerCC32XX_Object timerCC3220SObjects[CC3220S_LAUNCHXL_TIMERCOUNT];
    
    const TimerCC32XX_HWAttrs timerCC3220SHWAttrs[CC3220S_LAUNCHXL_TIMERCOUNT] = {
        {
            .baseAddress = TIMERA1_BASE,
            .subTimer = TimerCC32XX_timer32,
            .intNum = INT_TIMERA1A,
            .intPriority = ~0
        },
        {
            .baseAddress = TIMERA2_BASE,
            .subTimer = TimerCC32XX_timer32,
            .intNum = INT_TIMERA2A,
            .intPriority = ~0
        },
    };
    
    const Timer_Config Timer_config[CC3220S_LAUNCHXL_TIMERCOUNT] = {
        {
            .fxnTablePtr = &TimerCC32XX_fxnTable,
            .object = &timerCC3220SObjects[CC3220S_LAUNCHXL_TIMER0],
            .hwAttrs = &timerCC3220SHWAttrs[CC3220S_LAUNCHXL_TIMER0]
        },
        {
            .fxnTablePtr = &TimerCC32XX_fxnTable,
            .object = &timerCC3220SObjects[CC3220S_LAUNCHXL_TIMER1],
            .hwAttrs = &timerCC3220SHWAttrs[CC3220S_LAUNCHXL_TIMER1]
        },
    };
    
    const uint_least8_t Timer_count = CC3220S_LAUNCHXL_TIMERCOUNT;
    
    /*
     *  =============================== UART ===============================
     */
    #include <ti/drivers/UART.h>
    #if TI_DRIVERS_UART_DMA
    #include <ti/drivers/uart/UARTCC32XXDMA.h>
    
    UARTCC32XXDMA_Object uartCC3220SDmaObjects[CC3220S_LAUNCHXL_UARTCOUNT];
    
    /* UART configuration structure */
    const UARTCC32XXDMA_HWAttrsV1 uartCC3220SDmaHWAttrs[CC3220S_LAUNCHXL_UARTCOUNT] = {
        {
            .baseAddr = UARTA0_BASE,
            .intNum = INT_UARTA0,
            .intPriority = (~0),
            .flowControl = UARTCC32XXDMA_FLOWCTRL_NONE,
            .rxChannelIndex = UDMA_CH8_UARTA0_RX,
            .txChannelIndex = UDMA_CH9_UARTA0_TX,
            .rxPin = UARTCC32XXDMA_PIN_57_UART0_RX,
            .txPin = UARTCC32XXDMA_PIN_55_UART0_TX,
            .ctsPin = UARTCC32XXDMA_PIN_UNASSIGNED,
            .rtsPin = UARTCC32XXDMA_PIN_UNASSIGNED,
            .errorFxn = NULL
        },
        {
            .baseAddr = UARTA1_BASE,
            .intNum = INT_UARTA1,
            .intPriority = (~0),
            .flowControl = UARTCC32XXDMA_FLOWCTRL_NONE,
            .rxChannelIndex = UDMA_CH10_UARTA1_RX,
            .txChannelIndex = UDMA_CH11_UARTA1_TX,
            .rxPin = UARTCC32XXDMA_PIN_08_UART1_RX,
            .txPin = UARTCC32XXDMA_PIN_07_UART1_TX,
            .ctsPin = UARTCC32XXDMA_PIN_UNASSIGNED,
            .rtsPin = UARTCC32XXDMA_PIN_UNASSIGNED,
            .errorFxn = NULL
        }
    };
    
    const UART_Config UART_config[CC3220S_LAUNCHXL_UARTCOUNT] = {
        {
            .fxnTablePtr = &UARTCC32XXDMA_fxnTable,
            .object = &uartCC3220SDmaObjects[CC3220S_LAUNCHXL_UART0],
            .hwAttrs = &uartCC3220SDmaHWAttrs[CC3220S_LAUNCHXL_UART0]
        },
        {
            .fxnTablePtr = &UARTCC32XXDMA_fxnTable,
            .object = &uartCC3220SDmaObjects[CC3220S_LAUNCHXL_UART1],
            .hwAttrs = &uartCC3220SDmaHWAttrs[CC3220S_LAUNCHXL_UART1]
        }
    };
    
    #else
    #include <ti/drivers/uart/UARTCC32XX.h>
    
    UARTCC32XX_Object uartCC3220SObjects[CC3220S_LAUNCHXL_UARTCOUNT];
    unsigned char uartCC3220SRingBuffer[CC3220S_LAUNCHXL_UARTCOUNT][32];
    
    /* UART configuration structure */
    const UARTCC32XX_HWAttrsV1 uartCC3220SHWAttrs[CC3220S_LAUNCHXL_UARTCOUNT] = {
        {
            .baseAddr = UARTA0_BASE,
            .intNum = INT_UARTA0,
            .intPriority = (~0),
            .flowControl = UARTCC32XX_FLOWCTRL_NONE,
            .ringBufPtr  = uartCC3220SRingBuffer[CC3220S_LAUNCHXL_UART0],
            .ringBufSize = sizeof(uartCC3220SRingBuffer[CC3220S_LAUNCHXL_UART0]),
            .rxPin = UARTCC32XX_PIN_57_UART0_RX,
            .txPin = UARTCC32XX_PIN_55_UART0_TX,
            .ctsPin = UARTCC32XX_PIN_UNASSIGNED,
            .rtsPin = UARTCC32XX_PIN_UNASSIGNED,
            .errorFxn = NULL
        },
        {
            .baseAddr = UARTA1_BASE,
            .intNum = INT_UARTA1,
            .intPriority = (~0),
            .flowControl = UARTCC32XX_FLOWCTRL_NONE,
            .ringBufPtr  = uartCC3220SRingBuffer[CC3220S_LAUNCHXL_UART1],
            .ringBufSize = sizeof(uartCC3220SRingBuffer[CC3220S_LAUNCHXL_UART1]),
            .rxPin = UARTCC32XX_PIN_08_UART1_RX,
            .txPin = UARTCC32XX_PIN_07_UART1_TX,
            .ctsPin = UARTCC32XX_PIN_UNASSIGNED,
            .rtsPin = UARTCC32XX_PIN_UNASSIGNED,
            .errorFxn = NULL
        }
    };
    
    const UART_Config UART_config[CC3220S_LAUNCHXL_UARTCOUNT] = {
        {
            .fxnTablePtr = &UARTCC32XX_fxnTable,
            .object = &uartCC3220SObjects[CC3220S_LAUNCHXL_UART0],
            .hwAttrs = &uartCC3220SHWAttrs[CC3220S_LAUNCHXL_UART0]
        },
        {
            .fxnTablePtr = &UARTCC32XX_fxnTable,
            .object = &uartCC3220SObjects[CC3220S_LAUNCHXL_UART1],
            .hwAttrs = &uartCC3220SHWAttrs[CC3220S_LAUNCHXL_UART1]
        }
    };
    #endif /* TI_DRIVERS_UART_DMA */
    
    const uint_least8_t UART_count = CC3220S_LAUNCHXL_UARTCOUNT;
    
    /*
     *  =============================== Watchdog ===============================
     */
    #include <ti/drivers/Watchdog.h>
    #include <ti/drivers/watchdog/WatchdogCC32XX.h>
    
    WatchdogCC32XX_Object watchdogCC3220SObjects[CC3220S_LAUNCHXL_WATCHDOGCOUNT];
    
    const WatchdogCC32XX_HWAttrs watchdogCC3220SHWAttrs[CC3220S_LAUNCHXL_WATCHDOGCOUNT] = {
        {
            .baseAddr = WDT_BASE,
            .intNum = INT_WDT,
            .intPriority = (~0),
            .reloadValue = 80000000 /* 1 second period at default CPU clock freq */
        }
    };
    
    const Watchdog_Config Watchdog_config[CC3220S_LAUNCHXL_WATCHDOGCOUNT] = {
        {
            .fxnTablePtr = &WatchdogCC32XX_fxnTable,
            .object = &watchdogCC3220SObjects[CC3220S_LAUNCHXL_WATCHDOG0],
            .hwAttrs = &watchdogCC3220SHWAttrs[CC3220S_LAUNCHXL_WATCHDOG0]
        }
    };
    
    const uint_least8_t Watchdog_count = CC3220S_LAUNCHXL_WATCHDOGCOUNT;
    
    
    #if defined (__SF_DEBUG__) || defined(__SF_NODEBUG__)
    #if defined(__TI_COMPILER_VERSION__)
    #pragma DATA_SECTION(Board_debugHeader, ".dbghdr")
    #pragma RETAIN(Board_debugHeader)
    #elif defined(__IAR_SYSTEMS_ICC__)
    #pragma location=".dbghdr"
    #elif defined(__GNUC__)
    __attribute__ ((section (".dbghdr")))
    #endif
    #if defined(__SF_DEBUG__)
    const uint32_t Board_debugHeader[] = {
        0x5AA5A55A,
        0x000FF800,
        0xEFA3247D
    };
    #elif defined (__SF_NODEBUG__)
    const uint32_t Board_debugHeader[] = {
        0xFFFFFFFF,
        0xFFFFFFFF,
        0xFFFFFFFF
    };
    #endif
    #endif
    

    Thank you,

    Regards

    Sanath Rai

  • Hi Sanath,

    Have you tried running the door lock code on a CC3220SF launchpad in addition to your custom board, and seeing if the launchpad also doesn't seem to enter LPDS? Isolating the cause of the problem will be key, and knowing if it's in the door lock code or something to do with your hardware will be very useful.

    Regards,
    Michael

  • Hi Michael,

    I have run my code in cc3220sf launch pad but i have not checked whether it's going to LPDS mode or not.

    I will check that and update you.

    While checking the power consumption in cc3220sf launchpad i need to isolate  the emulator part right?  I need to check the power across cc3220sf ?

    Regards

    Sanath Rai

  • Hi Sanath,

    Yes, isolating the emulator is required. See section 3.2.3 of the TI design guide for test setup to replicate our power measurements on the launchpad setup.

    Regards,

    Michael

  • Hi Michael,

    Ok ,will do it and update you.

    Regards

    Sanath

  • Hello Michael,

    We tested the same set up in CC3220SF launchpad .Even here its taking 20mA. there is no difference . We made the setup same as mentioned in the document powering only cc3220sf and serial flash.

    After that  i made one more test 

    In my application i am using UART for communication with another host controller for our application.

    for the test i just removed it(commented the whole uart part) and after that when i dumped the code the current consumption reduced to micro amps .that means the UART is not allowing it to go to LPDS.

    But for my application UART is one of the main feature .

    As i just read about LPDS  that

    During LPDS the internal GPIO module is powered off, and special periphery logic is used instead to detect the trigger and wake thedevice. No GPIO interrupt service routine will be triggered in this case (even if an ISR is configured, and used normally to detect GPIO  interrupts when not in LPDS). This function can be used in lieu of a GPIO ISR, to take specific action upon LPDS wakeup.

    Only one GPIO {2,4,11,13,17,24,26} can be specified as a wake source for Shutdown. 

    So how can i use GPIO interrupts and UART in my application in LPDS mode?

    If not LPDS we can use sleep mode where it wakes from sleep whenever an interrupt hits unlike LPDS where it wakes only on network interrupts ,some chosen GPIOs and LPDS wake timer it seems.

    Regards

    Sanath

  • HI Michael,

    Here is a update regarding LPDS.

    As i mentioned in my earlier post after i commented out UART for the meantime the cc3220 is going to LPDS

    Yesterday i used GPIO13 to trigger the wake up from LPDS ,there inside that callback function  i again disabled the policy by using Power_disablePolicy(); function and then i used the other GPIO interrupt where  after the completion of task inside that ISR i enabled the policy again using Power_enablePolicy(); so that worked out for me for using GPIO Interrupts.

    But the concern is using UART for me . whenever i initialize the UART in the beginning the CC3220 is not going to LPDS.

    after that I tried to do the same thing where i disabled policy by Power_disablePolicy(); when GPIO13 is triggered and then initialized UART after that i transmitted data using uart_write()function and then enabled policy using Power_enablePolicy(); but here its not going to LPDS again.

    How to use UART in LPDS mode i am confused now?

    Regards

    Sanath

  • Hello Michael,

    Here is an update about LPDS.

    The issue was with UART receive call back which was not allowing the MCU to go to the idle state that's why its was not entering LPDS mode i guess.

    i disabled the receive call back initially and enabled only when i require it and now its going to the LPDS mode.

    The current consumption is low now,we will do further testing.

    Thank you for the support.

    Regards

    Sanath