Other Parts Discussed in Thread: CC3120, CC3100
Hello,
The SWRU457A is incorrect.
The doc shows this image:
However, P1, P2, P3, and P4 are NOT the same as my recently purchased board (< 2 months direct from TI). The 5 and 3.3V lines are not on the same labeled P1, P3 (they are physically in the same place)
This is an image of my board:
Furthermore, the jumper numbers are not correct either. J8 is not correctly labeled
So, can I reply on the switches being correct? At least some of this I can decipher with a simple DVM and the schematic...
Is there CORRECT documentation out there to match my board?
Do I need to worry about any other incorrect doc?