This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1831MOD: WL1831MOD

Part Number: WL1831MOD
Other Parts Discussed in Thread: WL1831

Hello,

Checking the signal integrity on SDIO (WiFi HCI) & UART (BT HCI) inputs of WL1381MOD, we found some over/undershoots of 0.5~0.6V above 1.8V = Vio. WIth 33R series res they are limited to 0.3V.

The datasheet is rather strict: 

- absolute max values: VDD_IO for CLK_IN (SDIO clock) and VDD_IO+0.5V for other pins.

- recommended values:  max Vih = VDD_IO

If we increase further the series res, we are afraid of degrading the rise time and get a not-steep-enough clock or data rise...

Question : is this 0.3V  over/undershoot acceptable considering it is only a transient violation of the spec ? Could this really impact long term reliability of the WL1831 ?

Thanks a lot for your support

Thomas

  • Hello,

    One more thing: we did not implement a series res on the signal connected to UART input BT_HCI_RX_1V8 and the over/undershoot is greater : ~0.7V.

    The base of the triangle made by the overshoot is 6.5ns wide. 

    Question: if short violations are OK during over/undershoot, how much is acceptable ?

  • Hi Thomas,

    For the digital links, both SDIO and HCI/UART lines, the signa needs to be within the -0.5V to VIO + 0.5V. If you violate this there is potential damage that can occur within the device. These pins have ESD protection within the device and this has a potential to be triggered. We cannot guarantee reliability of the device it this is in violation.

    Thanks,

    Riz