Part Number: CC3135
Other Parts Discussed in Thread: WL1807MOD, WL1837MOD
Hi Team,
Do we have suitable WIFI for dual 2.5/5GHz and support 802.11 a/b/g/n/ac?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Amelie,
As Jan mentioned, there is no TI device that supports 802.11ac at the moment. The CC3x35 devices as well as the WL1807MOD and WL1837MOD support 2.4GHz+5GHz. and if your customer doesn't have a hard requirement for 802.11ac then those devices can be suitable. As 802.11ac is a higher power + throughput standard, it is typically not required by Wi-Fi devices that do not require high data transfer rates such as typical IoT devices.
Let me know if you need more clarification or have further questions on this topic.
Regards,
Michael