Other Parts Discussed in Thread: WL1271
Hello,
I am using a WL1835MOD in combination with an AM335x. I go into suspend when there is no activity because we are running from a battery:
echo mem > /sys/power/state
If i have just wi-fi enabled and connected then i can suspend and resume with no issues; however, if i also have bluetooth enabled then i get a kernel panic and must reboot.
I am running kernel version 4.14.70 from the Robert C. Nelson kernel.
wl18xx-fw-4.bin versions:
FRev 8.9.0.0.83
FRev 8.2.0.0.243
Bluetooth firmware: TIInit_11.8.32.bts
Here is the panic output:
~ # echo mem > /sys/power/state
[ 215.844719] PM: suspend entry (deep)
[ 215.848792] PM: Syncing filesystems ... done.
[ 215.868400] Freezing user space processes ... (elapsed 0.002 seconds) done.
[ 215.879065] OOM killer disabled.
[ 215.882601] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) do
ne.
[ 215.892220] Suspending console(s) (use no_console_suspend to debug)
[ 215.900850] wlan0: deauthenticating from 88:15:44:ac:a3:28 by local choice (R
eason: 3=DEAUTH_LEAVING)
[ 215.950719] wlcore: down
[ 215.951384] queueing ieee80211 work while going to suspend
[ 215.975029] Timekeeping got suspended
[ 215.975029] pm33xx pm33xx: PM: Successfully put all powerdomains to target st
ate
[ 216.203314] mmc1: error -110 during resume (card was removed?)
[ 216.437873] Crashed from drivers/net/wireless/ti/wlcore/sdio.c on line 145
[ 216.437889] ------------[ cut here ]------------
[ 216.437962] WARNING: CPU: 0 PID: 2233 at drivers/net/wireless/ti/wlcore/sdio.
c:145 wl12xx_sdio_raw_write+0xdc/0x198 [wlcore_sdio]
[ 216.437972] Modules linked in: ipt_MASQUERADE nf_nat_masquerade_ipv4 iptable_
nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipv4 nf_nat nf_conntrack ip_tables x
_tables wl18xx wlcore wlcore_sdio spi_qrsdream pm33xx usb_f_midi usb_f_uac2 u_au
dio libcomposite [last unloaded: spi_omap2_mcspi]
[ 216.438158] CPU: 0 PID: 2233 Comm: kworker/u2:8 Not tainted 4.14.70.20+ #13
[ 216.438169] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 216.438210] Workqueue: events_unbound async_run_entry_fn
[ 216.438279] [<c0110ba4>] (unwind_backtrace) from [<c010d4e8>] (show_stack+0x2
0/0x24)
[ 216.438319] [<c010d4e8>] (show_stack) from [<c0a7cc20>] (dump_stack+0x20/0x28
)
[ 216.438370] [<c0a7cc20>] (dump_stack) from [<c0138708>] (__warn+0xe8/0x110)
[ 216.438407] [<c0138708>] (__warn) from [<c0138788>] (warn_slowpath_null+0x58/
0x60)
[ 216.438454] [<c0138788>] (warn_slowpath_null) from [<bf05930c>] (wl12xx_sdio_
raw_write+0xdc/0x198 [wlcore_sdio])
[ 216.438930] [<bf05930c>] (wl12xx_sdio_raw_write [wlcore_sdio]) from [<bf06ea5
8>] (wlcore_set_partition+0xd8/0x558 [wlcore])
[ 216.439405] [<bf06ea58>] (wlcore_set_partition [wlcore]) from [<bf06114c>] (w
l12xx_set_power_on+0x98/0x16c [wlcore])
[ 216.439857] [<bf06114c>] (wl12xx_set_power_on [wlcore]) from [<bf067f7c>] (wl
1271_op_add_interface+0x61c/0x964 [wlcore])
[ 216.440113] [<bf067f7c>] (wl1271_op_add_interface [wlcore]) from [<c0a05e10>]
(drv_add_interface+0x48/0x19c)
[ 216.440165] [<c0a05e10>] (drv_add_interface) from [<c0a3c9d8>] (ieee80211_rec
onfig+0x1a4/0x16c8)
[ 216.440221] [<c0a3c9d8>] (ieee80211_reconfig) from [<c0a26a00>] (ieee80211_re
sume+0x60/0x78)
[ 216.440275] [<c0a26a00>] (ieee80211_resume) from [<c09b4c88>] (wiphy_resume+0
x5c/0x188)
[ 216.440313] [<c09b4c88>] (wiphy_resume) from [<c05dc564>] (dpm_run_callback+0
x68/0x1fc)
[ 216.440344] [<c05dc564>] (dpm_run_callback) from [<c05dcd1c>] (device_resume+
0xc4/0x23c)
[ 216.440372] [<c05dcd1c>] (device_resume) from [<c05dcebc>] (async_resume+0x28
/0x54)
[ 216.440400] [<c05dcebc>] (async_resume) from [<c015cd38>] (async_run_entry_fn
+0x50/0x1e8)
[ 216.440446] [<c015cd38>] (async_run_entry_fn) from [<c0152db4>] (process_one_
work+0x138/0x47c)
[ 216.440481] [<c0152db4>] (process_one_work) from [<c01532d8>] (worker_thread+
0x198/0x59c)
[ 216.440518] [<c01532d8>] (worker_thread) from [<c01595b4>] (kthread+0x128/0x1
60)
[ 216.440559] [<c01595b4>] (kthread) from [<c0108d88>] (ret_from_fork+0x14/0x2c
)
[ 216.440578] ---[ end trace c6e94ada44e6ac22 ]---
[ 216.440610] wl1271_sdio mmc1:0001:2: sdio write failed (-110)
[ 216.909871] Crashed from drivers/net/wireless/ti/wlcore/sdio.c on line 145
[ 216.909886] ------------[ cut here ]------------
[ 216.909943] WARNING: CPU: 0 PID: 2233 at drivers/net/wireless/ti/wlcore/sdio.
c:145 wl12xx_sdio_raw_write+0xdc/0x198 [wlcore_sdio]
[ 216.909952] Modules linked in: ipt_MASQUERADE nf_nat_masquerade_ipv4 iptable_
nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipv4 nf_nat nf_conntrack ip_tables x
_tables wl18xx wlcore wlcore_sdio spi_qrsdream pm33xx usb_f_midi usb_f_uac2 u_au
dio libcomposite [last unloaded: spi_omap2_mcspi]
[ 216.910128] CPU: 0 PID: 2233 Comm: kworker/u2:8 Tainted: G W 4.1
4.70.20+ #13
[ 216.910139] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 216.910170] Workqueue: events_unbound async_run_entry_fn
[ 216.910222] [<c0110ba4>] (unwind_backtrace) from [<c010d4e8>] (show_stack+0x2
0/0x24)
[ 216.910257] [<c010d4e8>] (show_stack) from [<c0a7cc20>] (dump_stack+0x20/0x28
)
[ 216.910299] [<c0a7cc20>] (dump_stack) from [<c0138708>] (__warn+0xe8/0x110)
[ 216.910335] [<c0138708>] (__warn) from [<c0138788>] (warn_slowpath_null+0x58/
0x60)
[ 216.910380] [<c0138788>] (warn_slowpath_null) from [<bf05930c>] (wl12xx_sdio_
raw_write+0xdc/0x198 [wlcore_sdio])
[ 216.910730] [<bf05930c>] (wl12xx_sdio_raw_write [wlcore_sdio]) from [<bf06ea5
8>] (wlcore_set_partition+0xd8/0x558 [wlcore])
[ 216.911195] [<bf06ea58>] (wlcore_set_partition [wlcore]) from [<bf06114c>] (w
l12xx_set_power_on+0x98/0x16c [wlcore])
[ 216.911643] [<bf06114c>] (wl12xx_set_power_on [wlcore]) from [<bf067f7c>] (wl
1271_op_add_interface+0x61c/0x964 [wlcore])
[ 216.911894] [<bf067f7c>] (wl1271_op_add_interface [wlcore]) from [<c0a05e10>]
(drv_add_interface+0x48/0x19c)
[ 216.911935] [<c0a05e10>] (drv_add_interface) from [<c0a3c9d8>] (ieee80211_rec
onfig+0x1a4/0x16c8)
[ 216.911975] [<c0a3c9d8>] (ieee80211_reconfig) from [<c0a26a00>] (ieee80211_re
sume+0x60/0x78)
[ 216.912017] [<c0a26a00>] (ieee80211_resume) from [<c09b4c88>] (wiphy_resume+0
x5c/0x188)
[ 216.912051] [<c09b4c88>] (wiphy_resume) from [<c05dc564>] (dpm_run_callback+0
x68/0x1fc)
[ 216.912080] [<c05dc564>] (dpm_run_callback) from [<c05dcd1c>] (device_resume+
0xc4/0x23c)
[ 216.912108] [<c05dcd1c>] (device_resume) from [<c05dcebc>] (async_resume+0x28
/0x54)
[ 216.912136] [<c05dcebc>] (async_resume) from [<c015cd38>] (async_run_entry_fn
+0x50/0x1e8)
[ 216.912175] [<c015cd38>] (async_run_entry_fn) from [<c0152db4>] (process_one_
work+0x138/0x47c)
[ 216.912209] [<c0152db4>] (process_one_work) from [<c01532d8>] (worker_thread+
0x198/0x59c)
[ 216.912242] [<c01532d8>] (worker_thread) from [<c01595b4>] (kthread+0x128/0x1
60)
[ 216.912278] [<c01595b4>] (kthread) from [<c0108d88>] (ret_from_fork+0x14/0x2c
)
[ 216.912294] ---[ end trace c6e94ada44e6ac23 ]---
[ 216.912320] wl1271_sdio mmc1:0001:2: sdio write failed (-110)
[ 216.913890] wlcore: ERROR firmware boot failed despite 3 retries
[ 216.913910] Crashed from net/mac80211/util.c on line 1902
[ 216.913919] ------------[ cut here ]------------
[ 216.913954] WARNING: CPU: 0 PID: 2233 at net/mac80211/util.c:1902 ieee80211_r
econfig+0x1bc/0x16c8
[ 216.913962] Modules linked in: ipt_MASQUERADE nf_nat_masquerade_ipv4 iptable_
nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipv4 nf_nat nf_conntrack ip_tables x
_tables wl18xx wlcore wlcore_sdio spi_qrsdream pm33xx usb_f_midi usb_f_uac2 u_au
dio libcomposite [last unloaded: spi_omap2_mcspi]
[ 216.914129] CPU: 0 PID: 2233 Comm: kworker/u2:8 Tainted: G W 4.1
4.70.20+ #13
[ 216.914140] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 216.914162] Workqueue: events_unbound async_run_entry_fn
[ 216.914210] [<c0110ba4>] (unwind_backtrace) from [<c010d4e8>] (show_stack+0x2
0/0x24)
[ 216.914242] [<c010d4e8>] (show_stack) from [<c0a7cc20>] (dump_stack+0x20/0x28
)
[ 216.914279] [<c0a7cc20>] (dump_stack) from [<c0138708>] (__warn+0xe8/0x110)
[ 216.914314] [<c0138708>] (__warn) from [<c0138788>] (warn_slowpath_null+0x58/
0x60)
[ 216.914350] [<c0138788>] (warn_slowpath_null) from [<c0a3c9f0>] (ieee80211_re
config+0x1bc/0x16c8)
[ 216.914386] [<c0a3c9f0>] (ieee80211_reconfig) from [<c0a26a00>] (ieee80211_re
sume+0x60/0x78)
[ 216.914425] [<c0a26a00>] (ieee80211_resume) from [<c09b4c88>] (wiphy_resume+0
x5c/0x188)
[ 216.914458] [<c09b4c88>] (wiphy_resume) from [<c05dc564>] (dpm_run_callback+0
x68/0x1fc)
[ 216.914484] [<c05dc564>] (dpm_run_callback) from [<c05dcd1c>] (device_resume+
0xc4/0x23c)
[ 216.914512] [<c05dcd1c>] (device_resume) from [<c05dcebc>] (async_resume+0x28
/0x54)
[ 216.914539] [<c05dcebc>] (async_resume) from [<c015cd38>] (async_run_entry_fn
+0x50/0x1e8)
[ 216.914572] [<c015cd38>] (async_run_entry_fn) from [<c0152db4>] (process_one_
work+0x138/0x47c)
[ 216.914605] [<c0152db4>] (process_one_work) from [<c01532d8>] (worker_thread+
0x198/0x59c)
[ 216.914637] [<c01532d8>] (worker_thread) from [<c01595b4>] (kthread+0x128/0x1
60)
[ 216.914669] [<c01595b4>] (kthread) from [<c0108d88>] (ret_from_fork+0x14/0x2c
)
[ 216.914684] ---[ end trace c6e94ada44e6ac24 ]---
[ 216.915033] ------------[ cut here ]------------
[ 216.915075] WARNING: CPU: 0 PID: 2233 at net/mac80211/driver-ops.h:18 drv_rem
ove_interface+0x170/0x184
[ 216.915088] wlan0: Failed check-sdata-in-driver check, flags: 0x4
[ 216.915094] Modules linked in: ipt_MASQUERADE nf_nat_masquerade_ipv4 iptable_
nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipv4 nf_nat nf_conntrack ip_tables x
_tables wl18xx wlcore wlcore_sdio spi_qrsdream pm33xx usb_f_midi usb_f_uac2 u_au
dio libcomposite [last unloaded: spi_omap2_mcspi]
[ 216.915257] CPU: 0 PID: 2233 Comm: kworker/u2:8 Tainted: G W 4.1
4.70.20+ #13
[ 216.915267] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 216.915290] Workqueue: events_unbound async_run_entry_fn
[ 216.915334] [<c0110ba4>] (unwind_backtrace) from [<c010d4e8>] (show_stack+0x2
0/0x24)
[ 216.915364] [<c010d4e8>] (show_stack) from [<c0a7cc20>] (dump_stack+0x20/0x28
)
[ 216.915401] [<c0a7cc20>] (dump_stack) from [<c0138708>] (__warn+0xe8/0x110)
[ 216.915436] [<c0138708>] (__warn) from [<c0138828>] (warn_slowpath_fmt+0x48/0
x50)
[ 216.915473] [<c0138828>] (warn_slowpath_fmt) from [<c0a06274>] (drv_remove_in
terface+0x170/0x184)
[ 216.915508] [<c0a06274>] (drv_remove_interface) from [<c0a1bf98>] (ieee80211_
do_stop+0x708/0x8b0)
[ 216.915539] [<c0a1bf98>] (ieee80211_do_stop) from [<c0a1c160>] (ieee80211_sto
p+0x20/0x28)
[ 216.915571] [<c0a1c160>] (ieee80211_stop) from [<c0801e78>] (__dev_close_many
+0x98/0xd8)
[ 216.915600] [<c0801e78>] (__dev_close_many) from [<c0801f48>] (dev_close_many
+0x90/0x120)
[ 216.915630] [<c0801f48>] (dev_close_many) from [<c08046ec>] (dev_close+0x68/0
x8c)
[ 216.915666] [<c08046ec>] (dev_close) from [<c09b3dbc>] (cfg80211_shutdown_all
_interfaces+0x44/0xc8)
[ 216.915708] [<c09b3dbc>] (cfg80211_shutdown_all_interfaces) from [<c0a3a420>]
(ieee80211_handle_reconfig_failure+0xd4/0xd8)
[ 216.915746] [<c0a3a420>] (ieee80211_handle_reconfig_failure) from [<c0a3cb74>
] (ieee80211_reconfig+0x340/0x16c8)
[ 216.915782] [<c0a3cb74>] (ieee80211_reconfig) from [<c0a26a00>] (ieee80211_re
sume+0x60/0x78)
[ 216.915818] [<c0a26a00>] (ieee80211_resume) from [<c09b4c88>] (wiphy_resume+0
x5c/0x188)
[ 216.915850] [<c09b4c88>] (wiphy_resume) from [<c05dc564>] (dpm_run_callback+0
x68/0x1fc)
[ 216.915878] [<c05dc564>] (dpm_run_callback) from [<c05dcd1c>] (device_resume+
0xc4/0x23c)
[ 216.915904] [<c05dcd1c>] (device_resume) from [<c05dcebc>] (async_resume+0x28
/0x54)
[ 216.915932] [<c05dcebc>] (async_resume) from [<c015cd38>] (async_run_entry_fn
+0x50/0x1e8)
[ 216.915964] [<c015cd38>] (async_run_entry_fn) from [<c0152db4>] (process_one_
work+0x138/0x47c)
[ 216.915998] [<c0152db4>] (process_one_work) from [<c01532d8>] (worker_thread+
0x198/0x59c)
[ 216.916030] [<c01532d8>] (worker_thread) from [<c01595b4>] (kthread+0x128/0x1
60)
[ 216.916064] [<c01595b4>] (kthread) from [<c0108d88>] (ret_from_fork+0x14/0x2c
)
[ 216.916078] ---[ end trace c6e94ada44e6ac25 ]---
[ 216.926855] dpm_run_callback(): wiphy_resume+0x0/0x188 returns -110
[ 216.927111] PM: Device phy0 failed to resume async: error -110
[ 217.984777] OOM killer enabled.
[ 217.988183] Restarting tasks ... done.
[ 218.000459] PM: suspend exit
~ # [ 218.434031] Crashed from drivers/net/wireless/ti/wlcore/sdio.c on line 14
5
[ 218.441373] ------------[ cut here ]------------
[ 218.446377] WARNING: CPU: 0 PID: 1754 at drivers/net/wireless/ti/wlcore/sdio.
c:145 wl12xx_sdio_raw_write+0xdc/0x198 [wlcore_sdio]
[ 218.458759] Modules linked in: ipt_MASQUERADE nf_nat_masquerade_ipv4 iptable_
nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipv4 nf_nat nf_conntrack ip_tables x
_tables wl18xx wlcore wlcore_sdio spi_qrsdream pm33xx usb_f_midi usb_f_uac2 u_au
dio libcomposite [last unloaded: spi_omap2_mcspi]
[ 218.485599] CPU: 0 PID: 1754 Comm: ifplugd Tainted: G W 4.14.70.
20+ #13
[ 218.493846] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 218.500404] [<c0110ba4>] (unwind_backtrace) from [<c010d4e8>] (show_stack+0x2
0/0x24)
[ 218.508694] [<c010d4e8>] (show_stack) from [<c0a7cc20>] (dump_stack+0x20/0x28
)
[ 218.516392] [<c0a7cc20>] (dump_stack) from [<c0138708>] (__warn+0xe8/0x110)
[ 218.523803] [<c0138708>] (__warn) from [<c0138788>] (warn_slowpath_null+0x58/
0x60)
[ 218.532340] [<c0138788>] (warn_slowpath_null) from [<bf05930c>] (wl12xx_sdio_
raw_write+0xdc/0x198 [wlcore_sdio])
[ 218.543663] [<bf05930c>] (wl12xx_sdio_raw_write [wlcore_sdio]) from [<bf06ea5
8>] (wlcore_set_partition+0xd8/0x558 [wlcore])
[ 218.555954] [<bf06ea58>] (wlcore_set_partition [wlcore]) from [<bf06114c>] (w
l12xx_set_power_on+0x98/0x16c [wlcore])
[ 218.567656] [<bf06114c>] (wl12xx_set_power_on [wlcore]) from [<bf067f7c>] (wl
1271_op_add_interface+0x61c/0x964 [wlcore])
[ 218.579422] [<bf067f7c>] (wl1271_op_add_interface [wlcore]) from [<c0a05e10>]
(drv_add_interface+0x48/0x19c)
[ 218.589858] [<c0a05e10>] (drv_add_interface) from [<c0a1c5cc>] (ieee80211_do_
open+0x464/0x978)
[ 218.599052] [<c0a1c5cc>] (ieee80211_do_open) from [<c0a1cb40>] (ieee80211_ope
n+0x60/0x64)
[ 218.607792] [<c0a1cb40>] (ieee80211_open) from [<c0809480>] (__dev_open+0xb8/
0x118)
[ 218.615983] [<c0809480>] (__dev_open) from [<c0809818>] (__dev_change_flags+0
x188/0x1b0)
[ 218.624632] [<c0809818>] (__dev_change_flags) from [<c0809888>] (dev_change_f
lags+0x28/0x58)
[ 218.633676] [<c0809888>] (dev_change_flags) from [<c08a8f20>] (devinet_ioctl+
0x6bc/0x790)
[ 218.642360] [<c08a8f20>] (devinet_ioctl) from [<c08ab230>] (inet_ioctl+0x1c0/
0x1d0)
[ 218.650540] [<c08ab230>] (inet_ioctl) from [<c07e6170>] (sock_ioctl+0x84/0x30
4)
[ 218.658362] [<c07e6170>] (sock_ioctl) from [<c02a6480>] (do_vfs_ioctl+0x9c/0x
910)
[ 218.666368] [<c02a6480>] (do_vfs_ioctl) from [<c02a6d68>] (SyS_ioctl+0x74/0x8
4)
[ 218.674201] [<c02a6d68>] (SyS_ioctl) from [<c0108ca0>] (ret_fast_syscall+0x0/
0x54)
[ 218.682278] ---[ end trace c6e94ada44e6ac26 ]---
[ 218.687240] wl1271_sdio mmc1:0001:2: sdio write failed (-110)
[ 218.881523] Unhandled fault: external abort on non-linefetch (0x1008) at 0xe0
d8212c
[ 218.889646] pgd = db388000
[ 218.892522] [e0d8212c] *pgd=9c440811, *pte=47810653, *ppte=47810453
[ 218.899220] Internal error: : 1008 [#1] PREEMPT ARM
[ 218.904390] Modules linked in: ipt_MASQUERADE nf_nat_masquerade_ipv4 iptable_
nat nf_conntrack_ipv4 nf_defrag_ipv4 nf_nat_ipv4 nf_nat nf_conntrack ip_tables x
_tables wl18xx wlcore wlcore_sdio spi_qrsdream pm33xx usb_f_midi usb_f_uac2 u_au
dio libcomposite [last unloaded: spi_omap2_mcspi]
[ 218.931327] CPU: 0 PID: 1754 Comm: ifplugd Tainted: G W 4.14.70.
20+ #13
[ 218.939518] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 218.945964] task: dc3a9200 task.stack: db37c000
[ 218.950775] PC is at omap_hsmmc_set_bus_width+0x1c/0x8c
[ 218.956322] LR is at omap_hsmmc_set_ios+0x58/0x268
[ 218.961393] pc : [<c073f8e8>] lr : [<c07426b4>] psr: 20000013
[ 218.968029] sp : db37dbf8 ip : db37dc08 fp : db37dc04
[ 218.973525] r10: 00000000 r9 : 00000002 r8 : dc33dd68
[ 218.979025] r7 : 00000000 r6 : dc6401e4 r5 : dc640340 r4 : dc640000
[ 218.985892] r3 : e0d82100 r2 : dc640000 r1 : 00000001 r0 : dc640340
[ 218.992763] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 219.000270] Control: 10c5387d Table: 9b388019 DAC: 00000051
[ 219.006317] Process ifplugd (pid: 1754, stack limit = 0xdb37c210)
[ 219.012728] Stack: (0xdb37dbf8 to 0xdb37e000)
[ 219.017322] dbe0: db37d
c2c db37dc08
[ 219.025938] dc00: c07426b4 c073f8d8 c074265c dc640000 dc6401e4 00000001 dc3ec
808 dc33dd68
[ 219.034553] dc20: db37dc64 db37dc30 c072cfb0 c0742668 00000000 db37dc80 ffffb
098 c111b9c0
[ 219.043168] dc40: c111ccc0 c111b9c0 dc640000 00000015 00000001 dc3ec808 db37d
ca4 db37dc68
[ 219.051785] dc60: c072d34c c072cf18 c0a967ec c0192a70 db37dca4 00000000 c05d9
a0c dc3ec808
[ 219.060400] dc80: 00000004 dc640000 a0000013 dc3ec800 dc3ec808 dc33dd68 db37d
cc4 db37dca8
[ 219.069016] dca0: c072d580 c072d308 db205cd0 ffffffea dc2eaa00 dc3ec800 db37d
ce4 db37dcc8
[ 219.077632] dcc0: bf0591f8 c072d4fc db032d00 db032d00 db032d38 bf08d6c0 db37d
d04 db37dce8
[ 219.086248] dce0: bf0610f4 bf05916c dc33dc40 db032d00 ffffff92 db032d00 db37d
d64 db37dd08
[ 219.094864] dd00: bf067f7c bf0610c0 dc3a9200 dc33dc40 db032180 db032f74 dc33d
d48 dc33dd6c
[ 219.103478] dd20: 00000000 dc33dc40 00000000 00000000 dc33dc40 00000000 00000
000 dc33d4e8
[ 219.112094] dd40: db032420 db032420 dc33d4e0 00000000 db735d80 ffffffff db37d
d84 db37dd68
[ 219.120710] dd60: c0a05e10 bf06796c dc33d4e8 dc33d000 db032420 dc33d4e0 db37d
dc4 db37dd88
[ 219.129324] dd80: c0a1c5cc c0a05dd4 db032a00 00000000 db37ddc4 00000001 c0a1a
e98 dc33d4e0
[ 219.137940] dda0: c0c08db4 00000001 00001002 00000000 db735d80 c1103088 db37d
ddc db37ddc8
[ 219.146555] ddc0: c0a1cb40 c0a1c174 c0a1cae0 dc33d000 db37ddf4 db37dde0 c0809
480 c0a1caec
[ 219.155171] dde0: dc33d000 00001003 db37de24 db37ddf8 c0809818 c08093d4 db37d
e7c c0460098
[ 219.163786] de00: 00000001 dc33d000 00000144 00001002 db229e0c 00000000 db37d
e4c db37de28
[ 219.172402] de20: c0809888 c080969c 00000000 db37de74 db735d80 bea8e9b8 db229
e0c 00000000
[ 219.181017] de40: db37dec4 db37de50 c08a8f20 c080986c dc33d000 db37deb4 00000
000 dc33d000
[ 219.189633] de60: db229e0c 00000014 db229e00 00008914 db37de94 6e616c77 00000
030 00000000
[ 219.198246] de80: 00000000 00001003 00000000 00000000 00000000 c8ad147c db37d
ebc 00008914
[ 219.206861] dea0: ffffff24 c119fea8 bea8e9b8 bea8e9b8 db37c000 dbeae920 db37d
ed4 db37dec8
[ 219.215476] dec0: c08ab230 c08a8870 db37def4 db37ded8 c07e6170 c08ab07c db231
a80 db231a80
[ 219.224091] dee0: 00000000 bea8e9b8 db37df7c db37def8 c02a6480 c07e60f8 fffff
fff 00000000
[ 219.232706] df00: ffffffff 00000000 e16d8416 00eab5e0 5fcfc5ab 00000000 00000
001 db37df80
[ 219.241322] df20: 00000000 b6fc44c0 0000004e c0108e84 db37c000 00000000 db37d
f54 db37df48
[ 219.249937] df40: c0196ef4 c01959b4 db37df7c db37df58 c0196f34 db231a80 db231
a80 00000000
[ 219.258552] df60: bea8e9b8 00008914 db37c000 00000003 db37dfa4 db37df80 c02a6
d68 c02a63f0
[ 219.267168] df80: 000a91db 00000000 00b54008 00000036 c0108e84 00000000 00000
000 db37dfa8
[ 219.275784] dfa0: c0108ca0 c02a6d00 000a91db 00000000 00000003 00008914 bea8e
9b8 bea8e9b8
[ 219.284399] dfc0: 000a91db 00000000 00b54008 00000036 00000000 00b540b8 00000
000 000a912b
[ 219.293014] dfe0: 000bf300 bea8e9a4 00028b20 b6eb21bc 60000010 00000003 00000
000 00000000
[ 219.301645] [<c073f8e8>] (omap_hsmmc_set_bus_width) from [<c07426b4>] (omap_h
smmc_set_ios+0x58/0x268)
[ 219.311375] [<c07426b4>] (omap_hsmmc_set_ios) from [<c072cfb0>] (mmc_set_init
ial_state+0xa4/0x128)
[ 219.320822] [<c072cfb0>] (mmc_set_initial_state) from [<c072d34c>] (mmc_power
_up+0x50/0x1f4)
[ 219.329717] [<c072d34c>] (mmc_power_up) from [<c072d580>] (mmc_power_restore_
host+0x90/0x258)
[ 219.338724] [<c072d580>] (mmc_power_restore_host) from [<bf0591f8>] (wl12xx_s
dio_set_power+0x98/0xd0 [wlcore_sdio])
[ 219.350022] [<bf0591f8>] (wl12xx_sdio_set_power [wlcore_sdio]) from [<bf0610f
4>] (wl12xx_set_power_on+0x40/0x16c [wlcore])
[ 219.362085] [<bf0610f4>] (wl12xx_set_power_on [wlcore]) from [<bf067f7c>] (wl
1271_op_add_interface+0x61c/0x964 [wlcore])
[ 219.373751] [<bf067f7c>] (wl1271_op_add_interface [wlcore]) from [<c0a05e10>]
(drv_add_interface+0x48/0x19c)
[ 219.384110] [<c0a05e10>] (drv_add_interface) from [<c0a1c5cc>] (ieee80211_do_
open+0x464/0x978)
[ 219.393186] [<c0a1c5cc>] (ieee80211_do_open) from [<c0a1cb40>] (ieee80211_ope
n+0x60/0x64)
[ 219.401810] [<c0a1cb40>] (ieee80211_open) from [<c0809480>] (__dev_open+0xb8/
0x118)
[ 219.409883] [<c0809480>] (__dev_open) from [<c0809818>] (__dev_change_flags+0
x188/0x1b0)
[ 219.418410] [<c0809818>] (__dev_change_flags) from [<c0809888>] (dev_change_f
lags+0x28/0x58)
[ 219.427308] [<c0809888>] (dev_change_flags) from [<c08a8f20>] (devinet_ioctl+
0x6bc/0x790)
[ 219.435927] [<c08a8f20>] (devinet_ioctl) from [<c08ab230>] (inet_ioctl+0x1c0/
0x1d0)
[ 219.443994] [<c08ab230>] (inet_ioctl) from [<c07e6170>] (sock_ioctl+0x84/0x30
4)
[ 219.451703] [<c07e6170>] (sock_ioctl) from [<c02a6480>] (do_vfs_ioctl+0x9c/0x
910)
[ 219.459595] [<c02a6480>] (do_vfs_ioctl) from [<c02a6d68>] (SyS_ioctl+0x74/0x8
4)
[ 219.467307] [<c02a6d68>] (SyS_ioctl) from [<c0108ca0>] (ret_fast_syscall+0x0/
0x54)
[ 219.475289] Code: e52de004 e8bd4000 e5902004 e5903024 (e593102c)
[ 219.481711] ---[ end trace c6e94ada44e6ac27 ]---
~ #
~ #
~ # c0809818>] (__dev_change_flags) from [<c0809888>] (dev_change_flags+0x28/0x5
8)
[ 219.451703] [<c07e6170>] (sock_ioctl) from [<c02a6480>] (do_vfs_ioct-ash: syn
tax error: unexpected "("
~ # [ 219.427308] [<c0809888>] (dev_change_flags) from [<c08a8f20>] (devinet_io
ctl+0x6bc/0x790)
-ash: syntax error: unexpected "("
~ # [ 219.435927] [<c08a8f20>] (devinet_ioctl) from [<c08ab230>] (inet_ioctl+0x
1c0/0x1d0)
-ash: syntax error: unexpected "("
~ # [ 219.443994] [<c08ab230>] (inet_ioctl) from [<c07e6170>] (sock_ioctl+0x84/
0x304)
-ash: syntax error: unexpected "("
~ # [ 219.451703] [<c07e6170>] (sock_ioctl) from [<c02a6480>] (do_vfs_ioctl+0x9
c/0x910)
-ash: syntax error: unexpected "("
~ # [ 219.459595] [<c02a6480>] (do_vfs_ioctl) from [<c02a6d68>] (SyS_ioctl+0x74
/0x84)
-ash: syntax error: unexpected "("
~ # [ 219.467307] [<c02a6d68>] (SyS_ioctl) from [<c0108ca0>] (ret_fast_syscall+
0x0/0x54)
-ash: syntax error: unexpected "("
~ # [ 219.475289] Code: e52de004 e8bd4000 e5902004 e5903024 (e593102c)
-ash: syntax error: unexpected "("
~ # [ 219.481711] ---[ end trace c6e94ada44e6ac27 ]---
ash: missing ]
Any ideas what the problem could be?
Thanks,
Jarrod