Other Parts Discussed in Thread: TEST,
It is worth noting that: 1. When a program is interrupted abnormally, the next time to re run the program is normal operation and will not be interrupted. 2. If I reset the device hardware before running the program every time, there will be no abnormal interruption.
Program abnormal interrupt, interrupt to the following function position
* =============================== DMA ===============================
*/
#include <ti/drivers/dma/UDMACC32XX.h>
#include <ti/devices/cc32xx/inc/hw_ints.h>
#include <ti/devices/cc32xx/inc/hw_types.h>
#include <ti/devices/cc32xx/driverlib/rom_map.h>
#include <ti/devices/cc32xx/driverlib/udma.h>
/* Ensure DMA control table is aligned as required by the uDMA Hardware */
static tDMAControlTable dmaControlTable[64] __attribute__ ((aligned (1024)));
/* This is the handler for the uDMA error interrupt. */
static void dmaErrorFxn(uintptr_t arg)
{
int status = MAP_uDMAErrorStatusGet();
MAP_uDMAErrorStatusClear();
/* Suppress unused variable warning */
(void)status;
while (1);
}