Hi,
I'm trying to connect two Launchpad-CC3235SF via p2p mode with the network terminal example.
But I can't connect both devices in spite of using the 'p2pstart' command.
I found a forum link(below) that asked about the same issue, and tried to manually link it, as suggested in the link.
Unfortunately, device name is changing continuously(mysimplelink_xx, xx is random characters and it internally generated in NWP. see section 4.5.3.1 of Network processor User guide)
So, I can't connect the two devices again. (Because the device name changes when restarted)
What should I do? Please give me some advice.
Thanks.