Other Parts Discussed in Thread: CC3220S, UNIFLASH, CC3230S
Hi,
I am using CC3220s launchpad for programming the device with uniflash. It is working fine.
Now, I want to program the device with uniflash CLI. These are the steps I follow:
- Creating .sli image in uniflash.
- Connected my CC3220S Dev Kit to the PC.
- Executed the dslite.bat file in order to flash the .sli file I see the failure as seen below in the highlighted line.
>dslite --mode cc32xx image program --file Programming.sli
Executing the following command:
> SLImageCreator.exe image program --file Programming.sli
For more details and examples, please refer to the UniFlash Quick Start guide.
Config file (cfg.json) doesn't exist, using defaults
INFO:root:FTDI not detected, trying XDS
INFO:slbootloader.slbootloader:Connecting to device
INFO:slbootloader.slbootloader:Power off
INFO:slbootloader.slbootloader:Set break signal
INFO:slbootloader.slbootloader:Power on
INFO:slbootloader.slbootloader:Clear break signal
INFO:slbootloader.slbootloader:Connection succeeded
INFO:slbootloader.slbootloader:Received storage list
INFO:slbootloader.slbootloader:Received error : error number = -10275 , extended error = 4293
Traceback (most recent call last):
File "<string>", line 5189, in <module>
File "<string>", line 5185, in main
File "<string>", line 5157, in cmdline
File "<string>", line 4051, in command_image_program
File "<string>", line 2788, in program_image_from_sli
File "<string>", line 2882, in program_image
File "W:\slbootloader\slbootloader.py", line 793, in fs_programming
slbootloader.slbootloader.BootLoaderError:
Error: SLImageCreator.exe: fs_programming error: ret: -10275, ex_err: 4293 - FS_PROGRAMMING_ILLEGAL_FILE
SLImageCreator returned -1
- I also tried to run the SLImageCreator.exe directly without dslite file but I see the same error as above.