Other Parts Discussed in Thread: CC3220S, CC3220R, CC3220SF, CC3120
Hi,
We are using CC3220MODASF12MONR module as main controller. We are looking for optimum usage of power modes in our application. So far we are using the always connected scenario where the NWP is in Long Sleep Interval (LSI) mode. The max sleep parameter is set to 100 ms. The average current consumption in this mode is 27 mA.
Our application demands the current consumption to be in the order of uA. So as per the SWAS05B CC3220R, CC3220S, CC3220SF document, both the MCU and the NWP are to be in LPDS. We have the following questions:
- Will the MCU be able to perform other activities like data acquisition through ADC/SPI in LPDS mode? As per the SWRA502C CC3120, CC3220 SimpleLink Wi-Fi® Internet-on-a chip Networking Subsystem Power Management document, when the MCU is in LPDS mode all other logic except the hibernate
logic and top level logic are power gated. So does this mean other logic will not work?
- The Power Measurement example in the SDK puts the whole device to LPDS. Is there a possibility of sending just the MCU or NWP to LPDS. If so, how can it be achieved?
- We need the NWP to send data once every 100 ms and then sleep for rest of the time. Will it save power, if it remains connected to AP or should we sl_Start and sl_Stop everytime so that it reconnects to the AP and sends data through TCP sockets?
- The Power Management document says that the sl_WlanPolicySet configures the device management policy. So it means that it works on both MCU and NWP . Is that right?
- We are trying to configure the MCU LPDS, NWP Idle connected. In which configuration mode can be a power reduction solution?
Please guide us.
Looking forward your response!
Thanks,
Murali C