This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Capture Probe request packets CC31xx/CC32xx

Intellectual 445 points

Replies: 6

Views: 1425

I want to capture probe request and response packets. Would it be possible using CC31xx/CC32xx modules ?

  • Hi Hardik,

    Yes we can capture the probe request and response using cc3100 and cc3200.

    Please refer to the 'sls_sniffer_with_filters' example in CC3100 SDK.

    Regards,

    Ankur

    ----------------------------------------------------------------------------------------------------------
    Please click the 
    Verify Answer button on this post if it answers your question.
    ----------------------------------------------------------------------------------------------------------

  • In reply to Ankur Baranwal:

    Hello Ankur, 
    So probe requests can be captured without the CC3100 connected to any network (Just snooping out the probe request packets from the air) ?

  • In reply to Hardik Sanghavi:

    Hello Ankur, 

    Can we also get the RSSI values from the CC3100 modules for the probe request packets ?

    Thanks

    Hardik

  • In reply to Hardik Sanghavi:

    Yes, it provide RSSI as well.

  • Hi Hardik,

    Please let us know if above comment answers your question.

    Regards,

    Ankur

    ----------------------------------------------------------------------------------------------------------
    Please click the 
    Verify Answer button on this post if it answers your question.
    ----------------------------------------------------------------------------------------------------------

  • In reply to Ankur Baranwal:

    Dear Ankur,
    Could you please answer what is an average power consumtion of CC3100 wifi chip running the sls_sniffer_with_filters example?
    Are there any suggesions for battery operated Probe Request Sniffer to minimize power consumption of CC3100 chip?
    Thanks, Viktar

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.