This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Linux/WL1837MOD: WL1837MOD

Prodigy 160 points

Replies: 3

Views: 90

Part Number: WL1837MOD

Tool/software: Linux

We are studying if our device using the wl1837mod can implement MIMO on 5GHz.with the latest tag R8.7-SP3 of the kernel git.ti.com/wilink8-wlan/wl18xx.

  • Hi,
    WL1837MOD supports MIMO on 2.4 GHz band and not 5 GHz band.

    Thanks
    Saurabh
  • In reply to Saurabh Narang:

    Hi, Saurabh

    Thanks for the answer. so I'd have the following questions need be confirmation

    • if the tag R8.7-SP3 of wlconf able to config 2 antenna for 5G is dedicated for 5G diversity
    • if the antenna hardware be modified to meet requirements of 5G diversity, 2.4G MIMO function can still work?

    Best Regards

    Lei Dong

  • In reply to lei dong:

    Hi,
    WL18x7MOD hardware supports 5 GHz antenna diversity but not MIMO : www.ti.com/.../swaa161.pdf
    You cannot make h/w mods to the module to support 2x2 MIMO on 5GHz.

    Thanks
    Saurabh

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.