This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CC3220: CC3235, a new kid on the block

Intellectual 500 points

Replies: 3

Views: 290

Part Number: CC3220

Hello,

Just noticed that a new WiFi MCU is available. Sadly, there is no CPU performance data in the datasheet or the TRM (something like CC26xx "EEMBC CoreMark score"). Has anyone run any wide-recognized benchmark? In the past, I got some poor results with CC3220SF executing code from flash ( ), want to be sure that was resolved.

  • Guru 37585 points
    Hi,

    You should expect same performance as CC3220SF.

    Jan


    Please click to "Verify Answer", if your question was answered.

  • In reply to Jan D:

    Jan, is this opinion based on actual benchmarking?
  • Guru 37585 points

    In reply to Alexander Podshivalov:

    Hi,

    No. It is based on the my experiences and knowledge of internal structure of CC3235SF devices. I did not run any benchmark on CC3235SF.

    I can execute benchmark on my CC3235SF launchpad as you want. In this case provide me your benchmark project which can be imported into CCS (version 8.2).

    Jan


    Please click to "Verify Answer", if your question was answered.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.