This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 5
Views: 1606
Hello all,
I have developed a prototype for WiFi-based application using the CC3200R1M2 chip. Actually i had some questions regarding the CC3200R1M2 chip and serial flash:- 1)The SWRU369A says "The CC3200 solution combines a 2.4GHz Wi-Fi PHY/MAC and TCP/IP networking engine with a microcontroller, up to 256kB on-chip RAM (In XCC3200HZ and XCC3101GZ devices, only 176kb of RAM is available for applications) and a comprehensive range of peripherals." What is the rest 80kb used for in the case of XCC3200HZ ?? Will there be any difference if i use the examples from CC3200 SDK with CC3200R1M2 chip for my dedicated application ?? 2)The serial flash on the CC3200 LaunchXL launchpad comes with TI images and data which is not accessible to the user. In that case, if i use a serial flash bought from the vendor, will it have the TI images and data ?? Will it work in my prototype ?? 3)Does the NWP require a higher supply than 3.3V?? Please reply. Warm regards, Abhishek.
--------------------------------------------------------------------------------------------------------- Please click the Verify Answer button on this post if it answers your question. ---------------------------------------------------------------------------------------------------------
In reply to Siddaram Mathapathi:
In reply to Abhishek Ekhare: