Other Parts Discussed in Thread: UNIFLASH, CC3200
Hey all,
After compiling my project and attempting to load it with Uniflash, it fails because the file size is too big.
Exact error :
[19:12:12] ERROR: --- Invalid file size ---
[19:12:12] ERROR: Error, size if data (2252704) is too big to write
I've tried formatting the flash all sizes, 1MB, 2MB, ..., 16MB.
I have also tried increasing the "Max Size" of sys/mcuimg.bin to 0x30000 which is roughly 3MB
Also - 2,200kb seems huge for the amount of code I have in here - not very much.