This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

cc3100 without external flash

Prodigy 60 points

Replies: 6

Views: 862

Does anyone know if cc3100 can work without external flash? I want to use TCP/IP stack only. 

  • Hi,

    Not sure I understand exactly what you are trying to achieve. Can you elaborate more? are you going to use WiFi capabilities? if so, what exactly? station/AP? etc.

    I asking becasue without the serial flash the device is really lacking many functional features as all system and configurations are stored on the serial flash, also during run time.

    I'll provide some examples:

    1. the networking firmware is exectuted from ROM. It means you cannot load new service packs to fix bugs/issues discovered along the way
    2. with CC3100, you will not be able to boot as AP as this is a configuration stored on the flash
    3. you will not be able to set any WLAN profiles for connection, set IP address if you are working static IP, set any parameters for the services such as HTTP server, mDNS, etc
    4. SSL/TLS connection may fails if you are trying to authenticate the server as you cannot set date/time (also stored on the flash)
    5. and more...

    Shlomi

  • In reply to Shlomi Itzhak:

    I want to set cc3100 as station - I need to provide internet connection to other microcontroller.
  • In reply to Syl Kom:

    I don't want to use TLS/SSL I need only TCP/IP
  • In reply to Syl Kom:

    So unfortunately you need the serial flash as some system and configuration files are required for proper operations.

    Shlomi

  • In reply to Shlomi Itzhak:

    Hi,

    Did the above post answer your query? do you need more information?

    please verify the answer.

    Shlomi

  • In reply to Shlomi Itzhak:

    Hi,

    I am closing the thread, if issue still exist please open a new thread and add a link to this one for reference.

    Shlomi

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.