Other Parts Discussed in Thread: CC3200, UNIFLASH, ENERGIA
Hi,
We are developing a solution using CC3200 Launchpadxl to pull the data from Dspic33 and post it to webserver. We tested serial uart demo in the sdk using ccs and Tera Term, made sure it was working.
But when we connect CC3200 to Dspic33, CC3200 UART stopped working.
We made TTL level connections directly. That means Pin 57, Pin 55 was directly connected to dspic33FJ UART. Dspic UART is also 3.3V. LED's of the CC3200 is blinking, but no data was coming out of UART. We made sure Tx of CC3200 is connected to Rx of dspic33
After this, we disconnected the CC3200 and dspic connections and tried to analyze it, we found out that serial port was not responding. Even the basic weather app is not working. No data is coming on the Tera Term terminal now.
Kindly suggest how to wire UART to UART for CC3200, are we doing something wrong ?