This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does the wl127x Wilink chipset support WLAN Japan certification channel 14 for?

Does the wl127x chipsets support WLAN channel 14 usage in Japan.  We are testing the Diffusivity of the 11b data rates on channel 14 (2484MHz) and observing a failure.  

Diffusivity = (90% OBW)/1MHz (for 1 & 2 Mbps) = greater than 10 for 2484MHz, or greater than 5 for 2412-2472MHz

Diffusivity = (90% OBW)/1.375MHz (for 5.5 & 11 Mbps) = greater than 10 for 2484MHz, or greater than 5 for 2412-2472MHz

I measure the 90% OBW = ~9MHz for 11Mbps; Diffusivity = 6.54 and which is less than 10, therefore it fails.  

How do I get a bandwidth greater than 13.75MHz, or does this chipset not support Ch14 Japan usage?

Regards,

Mike