Customer is experiencing some "holes" in transmission when using the CC3000.
It seems like there is an interrupt latency every 200ms.
The delay occurs after sending HCI_CMND_SEND by SPI until an interrupt occurs on the CC3000.
SSID scan is disabled, is there other recommendations, that can be implemented to avoid this delay.
The delay is seen on the SPI communication:
BR
Anders