Part Number: WILINK-BT_WIFI-WIRELESS_TOOLS
I have Ti Arago linux running on BBB and am able to control Element14 WL1837 BT communication via Ti Bluetopia, but could not make HCITester work with the same wilink cape by following hcitester user guide.
I am certain that BT_EN = 1. I've tried connecting and disconnecting BBB HCI lines to Wilink when using HCITester + USB/Serial calbe, but failed in both cases. TIInit_11.8.32.bts is the initialization BT script I used.
In other words, after verifying BT working conditions of BBB+Element14 WL1837 cape, I replace BBB HCI lines with 3.3V USB/serial lines, but still leave the rest connections (jump wires) from BBB to wilink. When executing BT initialization script .bts, HCITester always times out in the step of setting baud rate at the very beginning.
What am I missing?
Thanks,
Buli