Part Number: WL1807MOD
Other Parts Discussed in Thread: WL1835MOD
Dear Experts,
could You please let us know, if WiLink8 WL1807Q supports SPI protocol instead of SDIO as the WLAN data interface to a uC/uP?
Many thanks and best regards,
Gregor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hari,
yes, for example connect WiLink8 WL1807Q to uP running Linux or Android or QNX OS.
Normally we use SDIO interface for the WLAN interface and UART for BT/BLE.
Question is: Does WiLink8 support usage of SPI instead of SDIO as WLAN interface to uP?
Thanks and best regards,
Gregor
Hi,
Actually it is supported with wilink8 in mainline linux using wlcore_spi.ko instead of wlcore_sdio:

For device tree bindings see:

BR,
Eyal
Hello,
is there any documentation on this feature besides the linux driver?
I'm specifically interested in the required connections for SPI mode between WL18xxMOD (in my case WL1835MOD) and the µC (NXP i.MX6UL). What to do with the SDIO-CMD and the SPI-CS lines? How does the WL18xx know that it is expected to communicate via SPI?
Can you please provide an example schematic or a connection diagram?
Best regards,
Ralf