Other Parts Discussed in Thread: CC3100, CC3200,
Tool/software: Starterware
Dear Support:
I am using a CC3120 with an MSP432 using the WiFi plugin v1.30 and trying to connect to my WLAN router using the code from the network_terminal example and it isn't always connecting - about 60% of the time. When it fails, I get the following error:
[ERROR] - FATAL ERROR: Sync loss detected n
[line:653, error code:-2005] Device error, please refer "DEVICE ERRORS CODES" section in errors.h
Network Terminal - Couldn't configure Network Processor
do you know what may be the problem? From looking up the error, I get the following:
/* API has been aborted due to an error detected by host driver */
#define SL_API_ABORTED (-2005)
but that doesn't tell me much. I have tried this with a couple different routers and getting the same result with about the same frequency of occurrence. Please advise of any thing I can try to fix this problem.
BTW - I use CC3100 and CC3200 a lot with these routers and have no issues with them connecting. Something going on that is unique to CC3120. I have also tried this with a CC3220 and getting the same problem with it connecting to these routers.
Thanks,
Tim