I know it's been posted before, but I've been having some trouble connecting to my AWS IoT... this is the serial output
CC3220 has connected to AP and acquired an IP address. IP Address: 192.168.0.18 Current time: Wed Jun 14 19:44:54 2017 Flashing certificate file ... successfully wrote file /cert/ca.der to flash Flashing certificate file ... successfully wrote file /cert/cert.der to flash Flashing certificate file ... successfully wrote file /cert/key.der to flash AWS IoT SDK Version 2.1.1- Connecting... ERROR: runAWSClient L#108 Error(-24) connecting to xxxxxx.us-east-2.amazonaws.com:8883 Subscribing... ERROR: runAWSClient L#126 Error subscribing (-13) ERROR: runAWSClient L#178 An error occurred in the loop. Error code = -13
As I understand it -24 is related to the root key, but I can't for the life of me figure out why it would be failing. My Dashboard shows successful connection attempts, but beyond that... nothing.
I'm migrating from Atmel's ASF's FreeRTOS implentation and so far find Ti-RTOS friendlier (never mind that I absolutely need to use this board for this project.) So... have some patience with me :)