Other Parts Discussed in Thread: TLV320AIC3106
Tool/software: Code Composer Studio
Hi,
My application needs to receive and send data to and from an audio codec TLV320AIC3106. I have configured I2S in CPU mode and could successfully read audio data from codec but unable to send data to codec. I probed an oscilloscope and there is no signal in I2S data out line. When I use I2SDataPut(I2S_BASE,I2S_STS_XDATA,ulDummy) the program gets stuck. Below is the I2S initialization code and I2S handler code and pinmux configuration. I am also attaching the schematic for you guys to make sure the pinmux configuration is correct.
void I2SIntHandler(void)
{
unsigned long ulStatus;
// Get the interrupt status
ulStatus = I2SIntStatus(I2S_BASE);
// Check if there was a Transmit interrupt; if so write next data into the tx buffer and acknowledge
// the interrupt
if(ulStatus & I2S_STS_XDATA)
{
I2SDataPutNonBlocking(I2S_BASE,I2S_DATA_LINE_0,ulDummy); // replaced ulDummy with 0x55 to see whether anything is coming,but no result
I2SIntClear(I2S_BASE,I2S_STS_XDATA);
}
// Check if there was a receive interrupt; if so read the data from the rx buffer and acknowledge
// the interrupt
if(ulStatus & I2S_STS_RDATA)
{
I2SDataGetNonBlocking( I2S_BASE, I2S_DATA_LINE_1,&ulDummy);
I2SIntClear(I2S_BASE,I2S_STS_RDATA);
audio_data_buffer[i2s_handler_index++]=ulDummy;
if(i2s_handler_index>=320){ // checking for 320 samples
i2s_handler_index=0;
i2sdatarecvdflag=1;
}
}
}
/*
//Initialize the I2S peripheral
*/
void AudioCaptureRendererConfigure(unsigned char bitsPerSample,
unsigned short bitRate,
unsigned char noOfChannels,
unsigned char RxTx,
unsigned char dma)
{
unsigned long bitClk;
// Initialising the McASP
//
MAP_PRCMPeripheralClkEnable(PRCM_I2S,PRCM_RUN_MODE_CLK);
PRCMPeripheralReset(PRCM_I2S);
bitClk = bitsPerSample * bitRate * noOfChannels;
dma=1;
if(bitsPerSample == 16)
{
MAP_PRCMI2SClockFreqSet((bitClk*10)); //(bitClk*10));//512000); (I2S_BASE,(bitClk*10),bitClk,I2S_SLOT_SIZE_16|
MAP_I2SConfigSetExpClk(I2S_BASE,(bitClk*10),bitClk,I2S_SLOT_SIZE_16| I2S_PORT_CPU); //(I2S_BASE,512000,bitClk,I2S_SLOT_SIZE_16|
}
MAP_I2SIntRegister(I2S_BASE, I2SIntHandler);
MAP_I2SIntEnable(I2S_BASE,I2S_INT_XDATA);
MAP_I2SIntEnable(I2S_BASE,I2S_INT_RDATA);
if(RxTx == I2S_MODE_RX_TX)
{
I2SSerializerConfig(I2S_BASE,I2S_DATA_LINE_1,I2S_SER_MODE_RX,
I2S_INACT_LOW_LEVEL);
}
if(RxTx & I2S_MODE_TX)
{
I2SSerializerConfig(I2S_BASE,I2S_DATA_LINE_0,I2S_SER_MODE_TX,
I2S_INACT_LOW_LEVEL);
}
if(RxTx == I2S_MODE_RX_TX)
{
MAP_I2SEnable(I2S_BASE,I2S_MODE_TX_RX_SYNC);
}
else if(RxTx & I2S_MODE_TX)
{
MAP_I2SEnable(I2S_BASE,I2S_MODE_TX_ONLY);
}
}
void
PinMuxConfig(void)
{
// Initialising the McASP
//
MAP_PRCMPeripheralClkEnable(PRCM_I2S,PRCM_RUN_MODE_CLK);
PRCMPeripheralReset(PRCM_I2S);
MAP_PinTypeI2S(PIN_64, PIN_MODE_7); //PIN_MODE_7
MAP_PinTypeI2S(PIN_62, PIN_MODE_13);
MAP_PinTypeI2S(PIN_63, PIN_MODE_7);
MAP_PinTypeI2S(PIN_50, PIN_MODE_6);
}
Thanks & regards,
Vishnu Pradeep