Part Number: CC3220SF-LAUNCHXL
Tool/software: TI-RTOS
Dear TI Team,
I am currently working on a project with CC3220SF-LAUNCHXL. I have questions about UART Read operation (callback mode).
Assume that I expect data frames of length 10 bytes and use the following code to enable UART Read.
UART_read(uartHandle, rxBuffer, 10);
If all incoming frames had the correct length, there would not be any issues. However, we know it's not always the case. (rxBuffer can store more than 10 bytes)
Scenario 1: shorter than expected
Imagine due to a power outage, the data sender manages to send only 5 bytes. In the case, UART Read will simply not return and wait for remaining bytes.
Then when another data frame with correct length arrives, UART Read will return, but the data is wrong (5 bytes of the first frame + 5 first bytes of the second frame).
Scenario 2: longer than expected
We may also received longer frames. Imagine if we receive 12 bytes, the current UART Read will return the correct data, but the next Read will be corrupted.
Trials:
I tried a timer with an isReading bool variable to prevent the scenario 1
and
close/open uartHandle before calling every next Read to prevent the scenario 2. (I should have called readCancel before)
However, both trials didn't work very well. They are not stable, usually after some iterations, they stops working.
If possible, I would be grateful if you could teach me how to handle these two situations.
Thanks in advance.