Part Number: CC3220
Other Parts Discussed in Thread: UNIFLASH
Hi,
We're trying to move to production with the C3220S and I am having trouble with the OTA key and Certificate I created according to these instructions from the TI Resource Explorer article about Wi-Fi OTA. dev.ti.com/.../
Generate the private key
openssl ecparam -name prime256v1 -genkey -out ota_vendor_key.pem
Generate the public certifcate
openssl req -new -x509 -key ota_vendor_key.pem -out ota_vendor_cert.pem -days 730
I have created these files as shown. Note that they are .pem files. Uniflash does accept the private key as a .pem. I remember reading that the CC3220 works with .pem files although I don't remember where I saw that. I have tried this with the cert changed to a der file, but that didn't help. I could not determine how to convert the key file to a der file, and maybe that would fix this.
I modified the OtaArchive.c file of the ota source as shown:
#define BUNDLE_CMD_FILE_NAME "ota.cmd"
#define BUNDLE_CMD_SIGNATURE_FILE_NAME "ota.sign"
#define OTA_CERTIFICATE_NAME "ota_vizco_cert.pem"
// #define OTA_CERTIFICATE_NAME "dummy_ota_vendor_cert.der"
#define BUNDLE_CMD_MAX_OBJECT_SIZE (1000)
Note that I changed the OTA_CERTIFICATE_NAME to ota_vizco_cert.pem which was generated by the (modified) openssl command above.
By the way, the OTA process works well with Dropbox when I use the "dummy" key and cert, but it fails to verify the a file signature when I try to use the certs I have generated.
This shows a snippet of the debug trace from the ota library.
[_BundleCmdFile_Parse] bundle cmd file=/sys/servicepack.ucf, sig_len=256, SHA_256_Digets=5c842c3139ecda90f0c15723f920a392b8d4d19f03281ee226359308f758f06e, cert=, secured=1, bundle=1
Signal Event 10-CONTINUE
Provisioning: State = OTA_RUN, Event=CONTINUE, Next State=OTA_RUN
OtaArchive_RunParseTar: parsing archive file header
OtaArchive_RunParseTar: skip block align RecvBufLen=863, SkipAlignSize=463
Signal Event 10-CONTINUE
Provisioning: State = OTA_RUN, Event=CONTINUE, Next State=OTA_RUN
OtaArchive_RunParseTar: parsing archive file header
OtaArchive_RunParseTar: FileType=0, FileName=ota.sign, FileSize=70
Signal Event 10-CONTINUE
Provisioning: State = OTA_RUN, Event=CONTINUE, Next State=OTA_RUN
[verifySignature] cert name=ota_vizco_cert.pem
[_BundleCmdSignatureFile_Parse] signature verification failed!
OtaArchive_RunParseTar: ERROR in _BundleCmdSignatureFile_Parse, Status=-12291
OTA_run: ERROR OtaArchive_RunParse, Status=-12291
_OtaCheckConsecutiveErrors: ConsecutiveOtaErrors=2/5, return only WARNNING
I made sure that I was compiling the ota library and I rebuilt the application and verified it was using the new ota.a library file.
I'm out of ideas to try. Could you help me with this?
Thanks,
Chuck