This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: OTA & Max Size Uniflash setting

Part Number: CC3200
Other Parts Discussed in Thread: UNIFLASH,

Hello,

I have a OTA question in UniFlash.

I create three user files:

1. mcuimg1.bin

2. mcuimg2.bin

3. mcuimg3.bin

Mcuimg1.bin is only updated by OTA.

I know that the updated image is not over max size configuration in UniFlash, but i don't know how to set.

mcuimg1.bin Max Size value can be set to 120k in UniFlash because the download image has a same free space at cc3200 flash?

mcuimg2.bin and  mcuimg3.bin are always set to 0. Is it ok?