Hello,
I want to implement a Watchdog in my application.
I have followed the "watchdog system demo" example. In my application it works fine if I flash it without the application bootloader... but for obvious reasons I need the application bootloader...
But when I flash application bootloader + my application, the watchdog is no longer triggering.
To be exact the watchdog does not trigger once Sl_Start(0,0,0) is called.
The code is working well if flashed alone but not if flashed along with application bootloader.
I'm aware that the WDT does not reset the NWP but here the WDT is not even restarting the application processor.
Any help is welcome.
Thanks :).