Hello
Based on the documentation, it is my understanding that the average RSSI from WlanRxStatGet is the average RSSI when sending data directly over the WLAN MAC layer without being connected to an Access Point. Is this correct?
If so, it seems that the average RSSI should not be used when wanting to know the RSSI for a given SSID (Access point). So, it seems that the network list has to be retrieved, find the desired SSID and then obtain the RSSI like demonstrated in the antenna selection example . Is this correct?
Also, what is the difference between the RSSI for given SSID and the average RSSI? Is the RSSI for a SSID an average or the current value at the time the network list is retrieved? Is it possible to obtain an average RSSI for a given SSID (Access Point)?
Thank you.
Steve