Part Number: CC3220
Hello Team,
Could you please advise me how the NWP behavior for the following scenarios:
the customer used CC3220 AT command layer without any profiles, he using AT+WlanConnect to specific SSID name (not MAC address) than sending a few bytes and goes to sleep.
what happens in case of multiple routers with the same SSID (different MAC).
since the customer does not control which router (AP) the device (cc3220) decided to connect, what would happen in that case?
will the device select the strongest AP signal (RSSI) and then connect or will select one AP randomly, for example, if we got 2 AP one -50 dBm and the second with -60 dBm what the devices choose to connect to.
According the customer it turns out that after a lot of tests he, when the cc3220 connected to a certain AP, is constantly repeating to connect to the same AP even if the specif AP is shut down for while (and there are other AP with the same SSID are online) it will try every time connect to the same AP. only after RESET, the device managed to select another working AP to connect to.
there is a way to add a threshold which limits via certain RSSI level to connect AP? or reach to a situation that every time the device tries to connect to SSID the RSSI will take into account for the selection of which AP to connect to?
I'll greatly appreciate any suggestion, Thanks.
Sincerely,
Shai