This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220: I/O Pin Protection Diode Current when driven below ground.

Part Number: CC3220


Hello,

I was examining the maximum ratings for the CC3220 I/O pins.  It seems there are some sort of protection diodes on the I/O pins because the min. rating is -0.5V.  I was wondering how much current the diode could handle.  This is only during a fault condition and I can keep it below 60uA with series resistance.  Just trying to not have to add another diode on the board.

Thanks