Other Parts Discussed in Thread: UNIFLASH
Hi,
We are working on CC3120, And its SDK plugin.
The CC3120 API replies with -2005 error API BLOCKED over the spi (seems like porting is not successful). Therefore we decided to first load the image through the UART and then check whether the image is properly loaded into cc3120 or not. My question is which file .bin, .hex. or .ucf file has to be moved into SRAM and Sflash of cc3120 using the bootloader mode. I managed to get through steps upto SRAM erase ( http://www.ti.com/lit/ug/swpa230a/swpa230a.pdf ), now i am wondering which file to load since i have limited memory on and off MCU STM32. and at what address of SRAM i should write the image on SRAM and Sflash.
I tried to search documentation but mostly are removed eg http://www.ti.com/tool/EMBEDDED-PROGRAMMING
Could you please suggest any documentation for the bootloading image via UART(since in production, uniflash tool usage will not be good idea) and getting API to work.
Thanks in advance.
Ravdeep