Part Number: CC3220MODA
Other Parts Discussed in Thread: CC3220SF
Tool/software: TI C/C++ Compiler
I created an internal flash region (FLASH_W) to save some data during code execution, to do so I have configured the CC3220SF_LAUNCHXL_TIRTOS.cmd as explained in

Just as follows:
MEMORY
{
/* Bootloader uses FLASH_HDR during initialization */
FLASH_HDR (RX) : origin = 0x01000000, length = 0x7FF /* 2 KB */
FLASH (RX) : origin = 0x01000800, length = 0x0BF800 /* 766KB */
FLASH_W (RWX) : origin = 0x010C0000, length = 0x40000 /* 256KB */
SRAM (RWX) : origin = 0x20000000, length = 0x00040000 /* 256KB */
}
It's working well, but just after the OTA process was completed, the whole internal flash gets erased (after the system reboot), as a result of I lost all my stored data in the FLASH_W region, Is there any way to prevent this to happen?
Thanks in advance.