Dear TI-Team,
I've already been running the SPI Test sample successfully but unfortunately I can't sl_DevGet to work properly.
I did some debugging and I can see that the actual hick-up is in sl_DevGet's
_SlReturnVal_t ret_val = _SlDrvCmdOp((_SlCmdCtrl_t *)&_SlDeviceGetCmdCtrl, &Msg, &CmdExt);
which returns -100 (SL_API_ABORTED, obviously)
Here's some logging output after sl_start:
SimpleLink started (mode: 0) before _SlDrvCmdOp _SlDrvCmdOp: call _SlDrvMsgWrite TX 21 43 34 12 TX 66 84 08 00 IRQ triggered NwpMaskInterrupt Interrupt is now masked TX 3c 2b 01 00 0c 00 00 20 TX 65 87 78 56 after _SlDrvResetCmdExt RX 7b b9 9b 57 7b b9 9b 56 RX cc 08 70 00 RX 70 00 00 00 RX 00 00 02 00 RX 18 00 58 00 RX 00 00 00 08 RX 02 00 00 00 RX 04 00 00 00 RX 00 00 00 00 RX 04 00 00 00 RX 02 00 06 2e RX 04 00 00 00 RX 04 00 00 00 RX 00 00 00 00 RX 02 00 00 00 RX 66 66 47 f3 RX 7b b9 9b 57 // this line repeats 27 times exited _SlDrvMsgReadCmdCtx after _SlDrvCmdOp: -100
As suggested in post I switchted to powering the boost from USB