This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: Large data delay problem when connecting some router

Part Number: CC3200


Hi  Team,

My customer meets problems when developing with CC3200.

Router:  Xiaomi R1C (dual-band AC wireless router, this problem does not occur in other routers); Other unknown type (from their customer)

Phenomenon: 

1.When connecting the above type of router, the power consumption of CC3200 will become significantly larger.

2.After connected,occasionally there will be a problem like: the server sends commands to the CC3200 with a large delay, but CC3200 uploading data is normal. Once this problem occurs, all the devices connected to the router will have this situation, and it will take a long time to recover. Once restored, the CC3200 will receive all the instructions that were previously unsuccessfully issued.

After connecting to the router, occasionally there will be "the server sends a command to the CC3200 with a large delay, but the upload data is normal." Once this problem occurs, all the devices connected to the router will have this situation, and it will take a long time to recover. Once restored, the CC3200 will receive all the instructions that were previously unsuccessfully issued.

Dose anyone have some clue for the strange phenomenon? Thanks a lot.


Best regards,
Viki Shi

  • Hi Viki Shi,

    When you mention that there is a significant increase in power consumption, is is possible to quantify this increase? What power mode is the customer operating in on the MCU and the NWP?
    For the delay issue when you say that "all the devices connected to the router will have this situation", do you mean all CC3200 devices or does this issue also affect other non-TI devices?

    To properly debug the issue, having the NWP and MAC logs from their device as it runs into the issue would be useful. Instructions can be found at this link:
    processors.wiki.ti.com/.../CC3100_&_CC3200_Capture_NWP_Logs
    To get MAC logs, follow the same steps, but mux out Pin60 as a UART output using MAP_PinTypeUART(PIN_60, PIN_MODE_1);

    Lastly, is the customer using their own custom board, and are they able to replicate this issue with a CC3200 launchpad?

    Regards,
    Michael
  • Hi Michael,

    This question is what I proposed!Thanks for your reply.

    1, When you mention that there is a significant increase in power consumption, is is possible to quantify this increase? What power mode is the customer operating in on the MCU and the NWP? 

    The current of the device with CC3200 connected to other routers is 800uA, the current is 3~4mA when it connects this router(xiaomi R1C). it Runs the normal power mode.

    2, For the delay issue when you say that "all the devices connected to the router will have this situation", do you mean all CC3200 devices or does this issue also affect other non-TI devices?

    All CC3200 devices occur this issue.I don't have any non-TI devices here.

    3,After doing other cross debugging, I will reply you if have any result.

  • Hi,

    The current you observe with the Xiaomi AP is indeed a bit high. Please acquire and provide the NWP and MAC logs, as this type of interoperability issue typically needs to be debugged through examining those logs.

    Regards,
    Michael
  • Hi Michael,

    I recently reappear this issue. The NWP and MAC logs are showed as follows:

    Issue: when mobilephone send out a command, CC3200  receive it very slow.(maybe dozens seconds,maybe few minutes)

    Thank you very much for your analysis!

    /**************************************NWP_LOG_PIN62********************************************/
    [17:03:52.412] 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 7B 1C 01 1F A8 C0 04 00 00 00 0D 00 00 00 
    [17:03:53.291] 2A 7B 1C 01 1F A8 C0 04 00 00 00 0E 00 00 00 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 
    [17:03:53.921] 2A 7B 1C 01 1F A8 C0 04 00 00 00 0F 00 00 00 37 31 80 24 04 00 00 89 02 00 00 F8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0A 3B 09 0A 76 22 00 A8 05 41 1A 77 22 4D 00 5C 05 2D 06 49 00 1A 78 22 00 00 5B 05 27 00 50 05 0A 79 22 00 00 27 00 1A 93 22 0C 00 6D 02 16 00 00 00 0A 8C 22 00 00 01 0E 1A 8D 22 01 00 53 01 00 00 00 00 1A 63 22 0E 00 8C 01 00 00 00 00 0A CC 21 5C 48 00 00 0A CA 21 2F 17 03 03 0A C7 21 27 00 7A 00 1A CB 21 27 00 E8 00 7A 00 57 01 12 BF 41 02 D4 0A CD 11 5B 02 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 00 0A 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 7B 1C 01 1F A8 C0 04 00 00 00 10 00 00 00 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 
    [17:03:55.182] 2A 7B 1C 01 1F A8 C0 04 00 00 00 11 00 00 00 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 7B 1C 01 1F A8 C0 04 00 00 00 12 00 00 00 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 
    [17:03:56.441] 2A 7B 1C 01 1F A8 C0 04 00 00 00 13 00 00 00 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 7B 1C 01 1F A8 C0 04 00 00 00 14 00 00 00 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 
    [17:03:57.701] 2A 7B 1C 01 1F A8 C0 04 00 00 00 15 00 00 00 
    [17:03:58.434] 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 7B 1C 01 1F A8 C0 04 00 00 00 16 00 00 00 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 
    [17:03:58.961] 2A 7B 1C 01 1F A8 C0 04 00 00 00 17 00 00 00 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 7B 1C 01 1F A8 C0 04 00 00 00 18 00 00 00 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 7C 14 18 A6 03 20 04 00 00 00 1B 36 19 20 18 00 00 08 00 1F 29 09 20 18 1F 29 09 01 94 0C 8C 19 02 01 00 0C 8D 11 08 03 0C 0C 20 03 01 00 00 1B 36 19 01 14 13 00 04 00 1F 29 09 01 14 1F 29 09 06 94 1B 36 19 06 14 00 00 04 00 1F 29 09 06 14 1A 2E 11 03 00 06 94 0C 8D 11 03 03 1A 9C 0A 10 27 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 1A 9C 0A E8 03 1A 9C 0A 10 27 34 A3 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 BD 3B FF BD 1A 9C 0A E8 03 34 A3 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 BD 3B FF BD 34 A3 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 BD 3B FF BD 0A 0B 09 14 1A 9C 0A 10 27 14 30 40 01 01 24 AB 60 03 00 2C 83 2C 83 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 1B 36 19 06 10 00 00 04 00 1F 29 09 06 10 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 03 00 03 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 03 00 03 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 1B 36 19 0A 10 08 00 0C 00 1B 7A 11 00 00 AA 43 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 37 31 80 92 04 00 00 F8 02 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 37 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 07 0A 21 1A 77 22 59 03 FE 04 4E 06 37 00 1A 78 22 00 00 F8 04 11 02 F3 04 0A 79 22 01 00 39 00 0A 93 22 00 B2 1C 00 0A 8C 22 00 2B 00 80 0A 8D 22 00 0B 00 00 1A 63 22 1F 00 44 02 00 00 00 00 0A CC 21 4D 41 00 00 0A CA 21 51 2C 03 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0B 00 25 01 0A CD 11 61 03 17 A7 80 01 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 00 14 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 42 3C FF BD 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 03 00 03 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 03 00 03 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 
    [17:04:05.650] 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 0A 0B 09 14 
    [17:04:14.141] 37 31 80 B1 04 00 00 17 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 01 00 0A 77 22 ED C7 F4 1E 0A 78 22 00 C7 C1 C4 0A 79 22 00 00 06 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 1A 63 22 04 00 BB 01 00 00 00 00 0A CC 21 53 5F 00 00 0A CA 21 6B 30 03 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0B 00 80 01 0A CD 11 63 02 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 00 1E 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:04:24.140] 37 31 80 B1 04 00 00 17 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 00 00 0A 77 22 00 00 00 15 0A 78 22 00 00 00 00 0A 79 22 00 00 00 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 0A 63 22 00 22 00 00 0A CC 21 57 63 00 00 0A CA 21 80 30 03 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0A 00 DC 01 0A CD 11 64 00 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 00 28 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:04:26.128] 0A 08 00 
    [17:04:34.140] 37 31 80 B1 04 00 00 17 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 00 00 0A 77 22 00 00 00 16 0A 78 22 00 00 00 00 0A 79 22 00 00 00 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 0A 63 22 00 1F 00 00 0A CC 21 5A 63 00 00 0A CA 21 96 30 03 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0A 00 C6 01 0A CD 11 64 00 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 00 32 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:04:44.139] 37 31 80 B1 04 00 00 17 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 00 00 0A 77 22 00 00 00 15 0A 78 22 00 00 00 00 0A 79 22 00 00 00 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 0A 63 22 00 1E 00 00 0A CC 21 5C 63 00 00 0A CA 21 AB 30 03 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0A 00 DC 01 0A CD 11 64 00 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 01 00 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:04:46.126] 0A 08 00 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 4A 3C FF BD 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 4A 3C FF BD 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 4A 3C FF BD 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 4A 3C FF BD 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 4A 3C FF BD 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 4A 3C FF BD 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 34 5F 80 B7 FF 00 00 F8 2A 00 00 5C 90 2A 79 4A 3C FF BD 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 1A 9C 0A E8 03 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 03 00 02 00 03 00 01 00 0A 5A 22 01 64 01 01 0F 6D 01 
    [17:04:50.157] 0A 9B 12 04 01 2A 5D 22 00 00 00 00 00 00 00 00 02 00 00 00 32 01 3C 00 2A 98 22 00 00 00 00 00 00 00 00 02 00 03 00 01 00 03 00 0A 5A 22 01 64 01 00 0F 6D 01 
    [17:04:54.138] 37 31 80 E7 04 00 00 4D 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 02 00 1A 77 22 9F 04 89 03 A2 04 15 00 1A 78 22 00 00 89 03 84 03 88 03 0A 79 22 00 00 49 00 0A 93 22 00 1F 14 00 0A 8C 22 00 00 00 1E 0A 8D 22 00 00 00 00 1A 63 22 1A 00 22 02 00 00 00 00 0A CC 21 59 47 00 00 0A CA 21 BE 31 04 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0B 00 0E 02 0A CD 11 63 01 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 01 0A 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:05:04.137] 37 31 80 E7 04 00 00 4D 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 00 00 0A 77 22 01 01 01 16 0A 78 22 00 01 01 00 0A 79 22 00 00 01 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 0A 63 22 00 23 00 00 0A CC 21 5A 63 00 00 0A CA 21 D3 32 04 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0A 00 DC 01 0A CD 11 64 00 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 01 14 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:05:14.136] 37 31 80 E7 04 00 00 4D 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 00 00 0A 77 22 00 00 00 15 0A 78 22 00 00 00 00 0A 79 22 00 00 00 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 0A 63 22 00 23 00 00 0A CC 21 5B 63 00 00 0A CA 21 E8 32 04 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0A 00 DC 01 0A CD 11 64 00 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 01 1E 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:05:20.703] 0A 08 00 
    [17:05:24.136] 37 31 80 E7 04 00 00 4D 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 00 00 0A 77 22 00 00 00 16 0A 78 22 00 00 00 00 0A 79 22 00 00 00 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 0A 63 22 00 20 00 00 0A CC 21 5C 63 00 00 0A CA 21 FE 32 04 04 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0A 00 C6 01 0A CD 11 64 00 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 01 28 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:05:34.135] 37 31 80 E7 04 00 00 4D 03 00 00 D8 B9 02 00 D8 FE 02 00 1F 11 0B 3C 83 17 5A 60 38 09 06 17 5C 80 01 0B 3B 09 0A 76 22 00 00 00 00 0A 77 22 00 00 00 15 0A 78 22 00 00 00 00 0A 79 22 00 00 00 00 0A 93 22 00 00 00 00 0A 8C 22 00 00 00 00 0A 8D 22 00 00 00 00 0A 63 22 00 1E 00 00 0A CC 21 5D 63 00 00 1A CA 21 13 01 32 00 04 00 04 00 0A C7 21 94 00 7A 00 1A CB 21 94 00 E8 00 7A 00 57 01 22 BF 41 0A 00 DC 01 0A CD 11 64 00 17 A7 80 00 00 00 00 0F 00 15 00 00 0F 01 15 00 25 0F 02 15 06 00 1A 11 18 01 00 00 00 DD 07 0A 10 18 00 01 32 0A 13 18 00 27 28 17 23 42 E7 00 37 32 80 4E 1A 02 00 00 00 00 00 00 00 00 00 0F 00 00 00 
    [17:05:40.702] 0A 08 00 
    
    
    /**************************************MAC_LOG_PIN60********************************************/
    [19:06:54.621] 08 00 80 3A 01 00 00 8F 27 F1 38 00 0F 8E 09 00 0C A7 1A 09 00 01 31 5F F2 38 00 AD 1A 09 00 DE 00 91 1F 09 00 00 00 0C 99 1F 09 00 1A 94 55 C9 06 00 A7 1F 09 00 AF AF 2F 30 00 BD 1F 09 00 0D 24 30 31 00 87 FE 08 00 01 1E AF 08 C2 25 85 08 00 A0 68 01 00 00 9F 8B F2 38 00 0F 8E 09 00 0C A7 1A 09 00 01 37 EF F3 38 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 B8 FE F3 38 F6 09 F4 38 86 1E 03 00 4B FE 08 00 0C C2 25 85 08 00 00 3C 01 00 00 2F 46 F4 38 00 0F 8E 09 00 0C A7 1A 09 00 02 F3 57 F4 38 00 AD 1A 09 00 DE E0 51 48 0A 00 00 04 01 04 03 18 58 F4 38 00 57 76 08 00 04 03 02 35 D9 75 08 00 B8 0E 41 01 B8 FE F3 38 C2 25 85 08 00 80 0F 06 00 00 09 5C F4 38 00 0F 8E 09 00 0C A7 1A 09 00 01 3B 2F FA 38 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 CB 3C FA 38 09 48 FA 38 13 3E 06 00 4D 60 08 00 00 00 01 27 00 C9 61 08 00 00 00 01 02 00 3D 61 08 00 00 00 01 00 4B FE 08 00 0D D2 25 85 08 00 E0 84 04 00 00 04 42 84 FA 38 00 0F 8E 09 00 0C A7 1A 09 00 01 1B DF FE 38 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 E3 F4 FE 38 20 00 FF 38 18 B8 04 00 4B FE 08 00 0E C2 25 85 08 00 80 7C 04 00 00 46 3C FF 38 00 0F 8E 09 00 0C A7 1A 09 00 01 18 8F 03 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 B1 95 03 39 EF A0 03 39 CE A0 04 00 4B FE 08 00 0F C2 25 85 08 00 60 8C 04 00 00 2A DD 03 39 00 0F 8E 09 00 0C A7 1A 09 00 01 32 3F 08 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 80 41 08 39 BD 4C 08 39 CF AB 04 00 4B FE 08 00 10 C2 25 85 08 00 C0 90 04 00 00 FA 88 08 39 00 0F 8E 09 00 0C A7 1A 09 00 01 2E EF 0C 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 3E F4 0C 39 7B FF 0C 39 BE B2 04 00 4B FE 08 00 11 C2 25 85 08 00 E0 8D 04 00 00 B7 3B 0D 39 00 0F 8E 09 00 0C A7 1A 09 00 01 2A 9F 11 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 B8 A2 11 39 F5 AD 11 39 7A AE 04 00 4B FE 08 00 12 C2 25 85 08 00 80 8F 04 00 00 32 EA 11 39 00 0F 8E 09 00 0C A7 1A 09 00 01 26 4F 16 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 65 55 16 39 A2 60 16 39 AD B2 04 00 4B FE 08 00 13 C2 25 85 08 00 A0 8C 04 00 00 DE 9C 16 39 00 0F 8E 09 00 0C A7 1A 09 00 01 23 FF 1A 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 D4 0C 1B 39 11 18 1B 39 6F B7 04 00 4B FE 08 00 14 C2 25 85 08 00 E0 84 04 00 00 4E 54 1B 39 00 0F 8E 09 00 0C A7 1A 09 00 01 1E AF 1F 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 AF C4 1F 39 EC CF 1F 39 DB B7 04 00 4B FE 08 00 15 C2 25 85 08 00 A0 7C 04 00 00 28 0C 20 39 00 0F 8E 09 00 0C A7 1A 09 00 01 1B 5F 24 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 9E 7D 24 39 DB 88 24 39 EF B8 04 00 4B FE 08 00 16 C2 25 85 08 00 40 73 04 00 00 17 C5 24 39 00 0F 8E 09 00 0C A7 1A 09 00 01 34 0F 29 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 47 23 29 39 84 2E 29 39 A9 A5 04 00 4B FE 08 00 17 C2 25 85 08 00 20 7E 04 00 00 BE 6A 29 39 00 0F 8E 09 00 0C A7 1A 09 00 01 32 BF 2D 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 A0 D2 2D 39 DD DD 2D 39 59 AF 04 00 4B FE 08 00 18 C2 25 85 08 00 C0 7E 04 00 00 1C 1A 2E 39 00 0F 8E 09 00 0C A7 1A 09 00 01 2E 6F 32 39 00 AD 1A 09 00 DE 00 87 FE 08 00 01 1E AF 08 C2 25 85 08 00 40 B1 04 00 00 04 9A 32 39 00 0F 8E 09 00 0C A7 1A 09 00 01 26 1F 37 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 CF 27 37 39 1A 33 37 39 2F 55 09 00 4B FE 08 00 19 C5 E7 03 0A 00 00 40 00 40 DC 46 79 37 39 F0 51 48 0A 00 1D 04 00 4D 03 20 3C 7A 37 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 D6 7A 37 39 00 8F A2 09 00 00 0C BB 17 08 00 04 ED 7A 37 39 0C 7D 58 0A 00 13 04 BF 37 39 00 AB A0 09 00 00 0C BB 17 08 00 04 1C BF 37 39 C5 E7 03 0A 00 00 20 00 20 01 81 FC 37 39 F0 51 48 0A 00 1D 04 02 C8 02 20 79 FD 37 39 00 45 87 08 00 02 D2 25 85 08 00 40 F4 03 00 00 04 42 FE 37 39 00 0F 8E 09 00 0C A7 1A 09 00 01 45 CF 3B 39 00 AD 1A 09 00 DD BD F3 7D 08 00 41 01 E4 D4 3B 39 21 E0 3B 39 15 AD 04 00 4B FE 08 00 1A C2 25 85 08 00 40 8D 04 00 00 5E 1C 3C 39 00 0F 8E 09 00 0C A7 1A 09 00 01 40 7F 40 39 00 AD 1A 09 00 DE 00 91 1F 09 00 00 00 0C 99 1F 09 00 1A 94 55 C9 06 00 A7 1F 09 00 AF AF 2F 30 00 BD 1F 09 00 0D 24 30 31 BD F3 7D 08 00 41 01 BA 84 40 39 F8 8F 40 39 D6 AF 04 00 4B FE 08 00 1B C2 25 85 08 00 60 8D 04 00 00 33 CC 40 39 00 0F 8E 09 00 0C A7 1A 09 00 01 1E 2F 45 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 AF 38 45 39 EC 43 45 39 F5 B3 04 00 4B FE 08 00 1C C2 25 85 08 00 40 89 04 00 00 2B 80 45 39 00 0F 8E 09 00 0C A7 1A 09 00 01 38 DF 49 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 3A E2 49 39 77 ED 49 39 8B A9 04 00 4B FE 08 00 1D C2 25 85 08 00 00 90 04 00 00 B4 29 4A 39 00 0F 8E 09 00 0C A7 1A 09 00 01 34 8F 4E 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 C1 93 4E 39 FF 9E 4E 39 87 B1 04 00 4B FE 08 00 1E C2 25 85 08 00 60 8E 04 00 00 39 DB 4E 39 00 0F 8E 09 00 0C A7 1A 09 00 01 31 3F 53 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 9E 49 53 39 DB 54 53 39 DD B5 04 00 4B FE 08 00 1F C2 25 85 08 00 40 88 04 00 00 18 91 53 39 00 0F 8E 09 00 0C A7 1A 09 00 01 2C EF 57 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 B8 FD 57 39 F5 08 58 39 1A B4 04 00 4B FE 08 00 20 C2 25 85 08 00 00 84 04 00 00 30 45 58 39 00 0F 8E 09 00 0C A7 1A 09 00 01 29 9F 5C 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 03 A7 5C 39 41 B2 5C 39 4B A9 04 00 4B FE 08 00 21 C2 25 85 08 00 00 8B 04 00 00 7D EE 5C 39 00 0F 8E 09 00 0C A7 1A 09 00 01 25 4F 61 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 26 59 61 39 63 64 61 39 23 B2 04 00 4B FE 08 00 22 C2 25 85 08 00 C0 88 04 00 00 A0 A0 61 39 00 0F 8E 09 00 0C A7 1A 09 00 01 21 FF 65 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 DC 06 66 39 19 12 66 39 B6 AD 04 00 4B FE 08 00 23 C2 25 85 08 00 40 8B 04 00 00 3B 4E 66 39 00 0F 8E 09 00 0C A7 1A 09 00 01 3B AF 6A 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 8A B9 6A 39 C6 C4 6A 39 AE B2 04 00 4B FE 08 00 24 C2 25 85 08 00 60 88 04 00 00 04 01 6B 39 00 0F 8E 09 00 0C A7 1A 09 00 01 36 5F 6F 39 00 AD 1A 09 00 DE F0 51 48 0A 00 1D 04 00 CA 02 20 EE 61 6F 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 93 62 6F 39 00 8F A2 09 00 00 0C BB 17 08 00 04 AB 62 6F 39 E0 51 48 0A 00 00 04 01 01 01 21 77 6F 39 00 57 76 08 00 01 01 02 35 D9 75 08 00 8A 09 41 01 8A B9 6A 39 00 87 FE 08 00 01 1E AF 08 E0 51 48 0A 00 00 04 01 04 03 07 9C 6F 39 00 57 76 08 00 04 03 02 35 D9 75 08 00 8A 09 41 01 8A B9 6A 39 BD F3 7D 08 00 41 01 9B F4 70 39 D6 FF 70 39 11 3B 06 00 4B FE 08 00 25 BD F3 7D 08 00 41 01 43 87 72 39 80 92 72 39 A8 92 01 00 4B FE 08 00 26 BD F3 7D 08 00 41 01 AC 27 74 39 E9 32 74 39 69 A0 01 00 4B FE 08 00 27 BD F3 7D 08 00 41 01 3E A4 75 39 7A AF 75 39 92 7C 01 00 4B FE 08 00 28 BD F3 7D 08 00 41 01 46 3C 77 39 82 47 77 39 08 98 01 00 4B FE 08 00 01 BD F3 7D 08 00 41 01 CF CD 78 39 0B D9 78 39 89 91 01 00 4B FE 08 00 02 BD F3 7D 08 00 41 01 C9 51 7A 39 06 5D 7A 39 FA 83 01 00 4B FE 08 00 01 BD F3 7D 08 00 41 01 9D ED 7B 39 D8 F8 7B 39 D4 9B 01 00 4B FE 08 00 02 BD F3 7D 08 00 41 01 53 86 7D 39 8D 91 7D 39 B6 98 01 00 4B FE 08 00 03 BD F3 7D 08 00 41 01 68 06 7F 39 A5 11 7F 39 15 80 01 00 4B FE 08 00 04 BD F3 7D 08 00 41 01 7F 92 80 39 BA 9D 80 39 17 8C 01 00 4B FE 08 00 05 BD F3 7D 08 00 41 01 DE 25 82 39 1B 31 82 39 5F 93 01 00 4B FE 08 00 06 0C 7D 58 0A 00 13 6E D2 82 39 00 AB A0 09 00 00 0C BB 17 08 00 04 86 D2 82 39 C5 E7 03 0A 00 00 20 00 20 01 10 10 83 39 F0 51 48 0A 00 1D 04 02 C8 02 20 F0 10 83 39 00 45 87 08 00 02 D1 25 85 08 00 E0 98 00 00 04 B9 11 83 39 00 0F 8E 09 00 0C A7 1A 09 00 01 32 AF 83 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 4C B3 83 39 97 BE 83 39 6E 8D 01 00 4B FE 08 00 07 C5 E7 03 0A 00 00 40 00 40 DC C1 04 84 39 F0 51 48 0A 00 1D 04 00 4D 03 20 B6 05 84 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 51 06 84 39 00 8F A2 09 00 00 0C BB 17 08 00 04 68 06 84 39 0C 7D 58 0A 00 13 76 43 85 39 00 AB A0 09 00 00 0C BB 17 08 00 04 90 43 85 39 BD F3 7D 08 00 41 01 59 4C 85 39 92 57 85 39 0D 99 01 E0 51 48 0A 00 00 04 01 01 01 05 6B 85 39 00 57 76 08 00 01 01 02 35 D9 75 08 00 59 0C 41 01 59 4C 85 39 00 4B FE 08 00 08 C5 E7 03 0A 00 00 20 00 20 01 6A 9E 85 39 F0 51 48 0A 00 1D 04 02 C8 02 20 4A 9F 85 39 00 45 87 08 00 02 D2 25 85 08 00 A0 31 01 00 00 04 18 A0 85 39 00 0F 8E 09 00 0C A7 1A 09 00 01 85 CF 86 39 00 AD 1A 09 00 DD BD F3 7D 08 00 41 01 B3 DC 86 39 FC E7 86 39 5A 90 01 00 4B FE 08 00 09 C5 E7 03 0A 00 00 40 00 40 DC 12 2F 87 39 F0 51 48 0A 00 1D 04 00 4D 03 20 0C 30 87 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 A2 30 87 39 00 8F A2 09 00 00 0C BB 17 08 00 04 BA 30 87 39 BD F3 7D 08 00 41 01 FE 69 88 39 3A 75 88 39 4B 8D 01 0C 7D 58 0A 00 13 C9 77 88 39 00 AB A0 09 00 00 0C BB 17 08 00 04 E2 77 88 39 00 4B FE 08 00 01 C5 E7 03 0A 00 00 20 00 20 01 FF BB 88 39 F0 51 48 0A 00 1D 04 02 C8 02 20 DF BC 88 39 00 45 87 08 00 02 D2 25 85 08 00 20 34 01 00 00 04 A8 BD 88 39 00 0F 8E 09 00 0C A7 1A 09 00 01 34 EF 89 39 00 AD 1A 09 00 DC BD F3 7D 08 00 41 01 24 F3 89 39 6F FE 89 39 26 89 01 00 4B FE 08 00 02 C5 E7 03 0A 00 00 40 00 40 DC 9A 44 8A 39 F0 51 48 0A 00 1D 04 00 4D 03 20 8F 45 8A 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 2A 46 8A 39 00 8F A2 09 00 00 0C BB 17 08 00 04 41 46 8A 39 0C 7D 58 0A 00 13 11 85 8B 39 00 AB A0 09 00 00 0C BB 17 08 00 04 2A 85 8B 39 BD F3 7D 08 00 41 01 98 87 8B 39 D3 92 8B 39 74 94 01 00 4B FE 08 00 03 C5 E7 03 0A 00 00 20 00 20 01 9A D9 8B 39 F0 51 48 0A 00 1D 04 02 C8 02 20 7A DA 8B 39 00 45 87 08 00 02 D2 25 85 08 00 A0 36 01 00 00 04 43 DB 8B 39 00 0F 8E 09 00 0C A7 1A 09 00 02 E1 EF 8C 39 00 AD 1A 09 00 DE 00 91 1F 09 00 00 00 0C 99 1F 09 00 1A 94 55 C9 06 00 A7 1F 09 00 AF AF 2F 30 00 BD 1F 09 00 0D 24 30 31 BD F3 7D 08 00 41 01 B3 1A 8D 39 FE 25 8D 39 1B 93 01 00 4B FE 08 00 04 C5 E7 03 0A 00 00 40 00 40 DC 34 6C 8D 39 F0 51 48 0A 00 1D 04 00 4D 03 20 29 6D 8D 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 C3 6D 8D 39 00 8F A2 09 00 00 0C BB 17 08 00 04 DA 6D 8D 39 BD F3 7D 08 00 41 01 6B A2 8E 39 A8 AD 8E 39 B8 87 01 0C 7D 58 0A 00 13 5C B9 8E 39 00 AB A0 09 00 00 0C BB 17 08 00 04 75 B9 8E 39 00 4B FE 08 00 05 C5 E7 03 0A 00 00 20 00 20 01 D5 F6 8E 39 F0 51 48 0A 00 1D 04 02 C8 02 20 B5 F7 8E 39 00 45 87 08 00 02 D2 25 85 08 00 A0 39 01 00 00 04 71 F8 8E 39 00 0F 8E 09 00 0C A7 1A 09 00 01 3B 2F 90 39 00 AD 1A 09 00 DB 00 87 FE 08 00 01 1E AF 08 C2 25 85 08 00 80 70 01 00 00 10 54 90 39 00 0F 8E 09 00 0C A7 1A 09 00 01 23 BF 91 39 00 AD 1A 09 00 DE 00 87 FE 08 00 02 1E AF 08 C2 25 85 08 00 00 67 01 00 00 28 ED 91 39 00 0F 8E 09 00 0C A7 1A 09 00 02 72 0A 93 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 37 51 93 39 82 5C 93 39 CC AE 04 00 4B FE 08 00 06 C5 E7 03 0A 00 00 40 00 40 DC 33 A9 93 39 F0 51 48 0A 00 1D 04 00 4D 03 20 31 AA 93 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 C3 AA 93 39 00 8F A2 09 00 00 0C BB 17 08 00 04 DB AA 93 39 E0 51 48 0A 00 00 04 01 04 03 92 E9 93 39 00 57 76 08 00 04 03 02 35 D9 75 08 00 37 01 41 01 37 51 93 39 0C 7D 58 0A 00 13 5D EA 93 39 00 AB A0 09 00 00 0C BB 17 08 00 04 76 EA 93 39 C5 E7 03 0A 00 00 20 00 20 01 DB 27 94 39 F0 51 48 0A 00 1D 04 02 C8 02 20 04 2C 94 39 00 45 87 08 00 02 D2 25 85 08 00 40 99 05 00 00 04 C9 2C 94 39 00 0F 8E 09 00 0C A7 1A 09 00 02 5F 06 95 39 00 AD 1A 09 00 DC E0 51 48 0A 00 00 04 01 01 01 0C 0E 95 39 00 57 76 08 00 01 01 02 35 D9 75 08 00 37 01 41 01 37 51 93 39 D2 25 85 08 00 20 65 01 00 00 04 FA 0E 95 39 00 0F 8E 09 00 0C A7 1A 09 00 01 3D 6F 96 39 00 AD 1A 09 00 D9 BD F3 7D 08 00 41 01 37 71 96 39 82 7C 96 39 00 20 03 F0 51 48 0A 00 1D 04 00 45 07 20 0B 91 96 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 31 92 96 39 00 8F A2 09 00 00 0C BB 17 08 00 04 8C 92 96 39 E0 51 48 0A 00 00 04 01 04 03 57 93 96 39 00 57 76 08 00 04 03 02 35 D9 75 08 00 37 01 41 01 37 71 96 39 BD F3 7D 08 00 41 01 36 01 98 39 73 0C 98 39 FF 8F 01 00 4B FE 08 00 01 BD F3 7D 08 00 41 01 39 91 99 39 76 9C 99 39 03 90 01 00 4B FE 08 00 02 0C 7D 58 0A 00 13 3F 04 9A 39 00 AB A0 09 00 00 0C BB 17 08 00 04 58 04 9A 39 C5 E7 03 0A 00 00 20 00 20 01 BB 41 9A 39 F0 51 48 0A 00 1D 04 02 C8 02 20 E4 45 9A 39 00 45 87 08 00 02 D2 25 85 08 00 40 7A 02 00 00 04 A9 46 9A 39 00 0F 8E 09 00 0C A7 1A 09 00 01 87 AF 9C 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 36 B1 9C 39 81 BC 9C 39 FD 1F 03 F0 51 48 0A 00 1D 04 00 1C 08 20 E8 CE 9C 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 88 CF 9C 39 00 8F A2 09 00 00 0C BB 17 08 00 04 9F CF 9C 39 00 4B FE 08 00 03 BD F3 7D 08 00 41 01 37 41 9E 39 74 4C 9E 39 01 90 01 00 4B FE 08 00 04 0C 7D 58 0A 00 13 01 0D 9F 39 00 AB A0 09 00 00 0C BB 17 08 00 04 19 0D 9F 39 C5 E7 03 0A 00 00 20 00 20 01 7F 4A 9F 39 F0 51 48 0A 00 1D 04 02 C8 02 20 C0 4E 9F 39 00 45 87 08 00 02 D2 25 85 08 00 20 1D 02 00 00 04 85 4F 9F 39 00 0F 8E 09 00 0C A7 1A 09 00 01 A2 5F A1 39 00 AD 1A 09 00 DE BD F3 7D 08 00 41 01 3B 61 A1 39 86 6C A1 39 04 20 03 F0 51 48 0A 00 1D 04 00 32 07 20 9B 7E A1 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 AE 7F A1 39 00 8F A2 09 00 00 0C BB 17 08 00 04 C6 7F A1 39 00 4B FE 08 00 05 BD F3 7D 08 00 41 01 3B F1 A2 39 78 FC A2 39 00 90 01 00 4B FE 08 00 06 0C 7D 58 0A 00 13 76 EE A3 39 00 AB A0 09 00 00 0C BB 17 08 00 04 8E EE A3 39 0C 7D 58 0A 00 13 B2 EF A3 39 00 8F A2 09 00 00 0C BB 17 08 00 04 FD 2B A4 39 BD F3 7D 08 00 41 01 42 81 A4 39 7F 8C A4 39 07 90 01 00 4B FE 08 00 07 BD F3 7D 08 00 41 01 02 11 A6 39 3F 1C A6 39 C0 8F 01 00 4B FE 08 00 08 BD F3 7D 08 00 41 01 26 A1 A7 39 63 AC A7 39 24 90 01 00 4B FE 08 00 09 BD F3 7D 08 00 41 01 FF 30 A9 39 3B 3C A9 39 D9 8F 01 00 4B FE 08 00 0A 00 87 FE 08 00 01 1E AF 08 BD F3 7D 08 00 41 01 02 51 AC 39 3E 5C AC 39 03 20 03 00 4B FE 08 00 0B 00 87 FE 08 00 01 1E AF 08 BD F3 7D 08 00 41 01 04 71 AF 39 41 7C AF 39 02 20 03 00 4B FE 08 00 0C BD F3 7D 08 00 41 01 09 01 B1 39 45 0C B1 39 05 90 01 00 4B FE 08 00 0D BD F3 7D 08 00 41 01 0C 91 B2 39 48 9C B2 39 03 90 01 00 4B FE 08 00 0E BD F3 7D 08 00 41 01 05 21 B4 39 42 2C B4 39 F9 8F 01 00 4B FE 08 00 0F BD F3 7D 08 00 41 01 0E B1 B5 39 4A BC B5 39 09 90 01 BD F3 7D 08 00 41 01 0B 41 B7 39 47 4C B7 39 FD 8F 01 00 4B FE 08 00 01 BD F3 7D 08 00 41 01 0F D1 B8 39 4C DC B8 39 04 90 01 00 4B FE 08 00 02 BD F3 7D 08 00 41 01 0E 61 BA 39 4B 6C BA 39 FF 8F 01 0C 7D 58 0A 00 13 37 82 BA 39 00 AB A0 09 00 00 0C BB 17 08 00 04 4F 82 BA 39 00 4B FE 08 00 03 C5 E7 03 0A 00 00 20 00 20 01 AE BF BA 39 F0 51 48 0A 00 1D 04 02 C8 02 20 F6 C3 BA 39 00 45 87 08 00 02 D2 25 85 08 00 20 D0 02 00 00 04 BB C4 BA 39 00 0F 8E 09 00 0C A7 1A 09 00 01 88 7F BD 39 00 AD 1A 09 00 DC BD F3 7D 08 00 41 01 0B 81 BD 39 56 8C BD 39 FD 1F 03 F0 51 48 0A 00 1D 04 00 1C 08 20 AB 9E BD 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 6F 9F BD 39 00 8F A2 09 00 00 0C BB 17 08 00 04 87 9F BD 39 00 4B FE 08 00 04 BD F3 7D 08 00 41 01 14 11 BF 39 51 1C BF 39 09 90 01 00 4B FE 08 00 05 BD F3 7D 08 00 41 01 11 A1 C0 39 4E AC C0 39 FD 8F 01 0C 7D 58 0A 00 13 31 C3 C0 39 00 AB A0 09 00 00 0C BB 17 08 00 04 49 C3 C0 39 00 4B FE 08 00 06 C5 E7 03 0A 00 00 20 00 20 01 AF 00 C1 39 F0 51 48 0A 00 1D 04 02 C8 02 20 EB 04 C1 39 00 45 87 08 00 02 D2 25 85 08 00 C0 2B 01 00 00 04 B0 05 C1 39 00 0F 8E 09 00 0C A7 1A 09 00 01 A3 2F C2 39 00 AD 1A 09 00 DC BD F3 7D 08 00 41 01 14 31 C2 39 5F 3C C2 39 03 90 01 00 F9 03 09 00 F0 51 48 0A 00 1D 04 00 AD 07 20 8E 4E C2 39 00 45 87 08 00 00 0C 7D 58 0A 00 13 25 50 C2 39 00 8F A2 09 00 00 0C BB 17 08 00 04 3D 50 C2 39 00 4B FE 08 00 01 BD F3 7D 08 00 41 01 13 C1 C3 39 50 CC C3 39 FF 8F 01 00 4B FE 08 00 02 00 5B FE 08 00 BD F3 7D 08 00 41 01 17 51 C5 39 54 5C C5 39 04 90 01 BD F3 7D 08 00 41 01 17 E1 C6 39 54 EC C6 39 00 90 01 00 4B FE 08 00 01 BD F3 7D 08 00 41 01 16 71 C8 39 53 7C C8 39 FF 8F 01

    MAC_LOG_PIN60
  • Hi,

    Thanks for coming back with those logs. However, could you kindly please provide the logs as a raw binary file? The text files that you have provided do not allow me to parse the logs with the tools I have.

    Thanks,
    Michael
  • Hi ,

    I assume that you have resolved your issue since I have not heard back from you. If not, feel free to post a response to this thread, or open a new thread regarding this issue.

    Regards,
    Michael