Part Number: CC3235SF
Other Parts Discussed in Thread: CC3220SF, , SYSBIOS
Tool/software: TI-RTOS
Dear Support:
I am porting over my CC3220SF projects to CC3235SF and using SDK v2.40 and running into a problem where a previous call Timestamp_get32(.) works with my previous versions of SDKs dating back to v1.50, but is failing with this newer SDK v2.40. Below are the libraries I am using in this CCS project:
${INHERITED_LIBRARIES}
ccs/m4/slnetsock_release.a
ccs/Release/slnetifwifi.a
ti/display/lib/display.aem4
ti/grlib/lib/ccs/m4/grlib.a
third_party/spiffs/lib/ccs/m4/spiffs.a
ti/drivers/lib/drivers_cc32xx.aem4
third_party/fatfs/lib/ccs/m4/fatfs.a
ccs/rtos/simplelink.a
ti/dpl/lib/dpl_cc32xx.aem4
ti/devices/cc32xx/driverlib/ccs/Release/driverlib.a
libc.a
However I found that the CCS project stairstepStopMode is using this Timestamp_get32() function and is using these libraries:
${COM_TI_SIMPLELINK_CC32XX_SDK_LIBRARIES}
ti/display/lib/display.aem4
ti/grlib/lib/ccs/m4/grlib.a
third_party/spiffs/lib/ccs/m4/spiffs.a
ti/drivers/lib/drivers_cc32xx.aem4
third_party/fatfs/lib/ccs/m4/fatfs.a
ti/dpl/lib/dpl_cc32xx.aem4
ti/devices/cc32xx/driverlib/ccs/Release/driverlib.a
libc.a
I am able to build with v2.40 using this CCS project. You can see that these libraries are also in the CCS project that I am using that is failing. Do you know what is going on here such that my CCS project is failing in the linking stage? Please see linking error that is displayed:
<Linking>
undefined first referenced
symbol in file
--------- ----------------
xdc_runtime_Timestamp_get32__E ./common/command_utils.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "sensor_3235.out" not built
>> Compilation failure
makefile:182: recipe for target 'sensor_3235.out' failed
Your thoughts?
Thanks,
Tim