Part Number: CC3200-LAUNCHXL
Other Parts Discussed in Thread: ENERGIA
Hello there,
Ive been trying to use the UART on pin number 3 and 4 by using serial for monitoring the received data and serial1 for connecting and controlling the hardware(GPS) but the by using serial1 i think the uart isnt active.
i see by connecting gps to putty that there is no data sent from the cc device .
I checked the hardware serial .h and .cpp file where in the cpp file there is serial1 functions mentioned but in the pins_energia file i see no pin initialized as uart only analog, timers and gpio's are initialized. So what can i do to make it work.
Serial1.begin(112500);
Serial.begin(19200);
delay(50);
Serial1.println("AT");
delay(1000);
Serial1.println("AT+QGNSSC?");
delay(1000);
Serial1.println("AT+QGNSSC=1");
delay(1000);
Serial1.println("AT+QGNSSTS?");
delay(1000);