Part Number: BOOSTXL-CC3135
Tool/software: TI-RTOS
Hi,
As the picture shows,I run the power_measurement demo,something changed as flow:
1、LSI delay set to 1s;
2、#define IP_ADDR_ALLOC_MODE STATIC_IP
3、disable the function alwaysConnected() ;
Connected AP Model is TP-LINK.:TL-WR8842N.
So,I didn't take the initiative to send messages.Then how to understand the waveform in the picture include so many peaks at the first and several peak sending packets likely after entered the LPDS? Please give me some explanation,thanks.
PS:Red circle 1 means the waveform after run the always connected mode,red circle 2 means waveform in the LPDS mode.