Other Parts Discussed in Thread: CC3220SF
Tool/software: TI-RTOS
Hi all,
I have a problem with the tcpEcho example. The board starts, connects to my Wifi environment, opens the socket 1000 and I can connect with a telnet client. I can send messages and receive the echo.
The program runs in a debug session (not flashed).
[NETAPP EVENT] IP Acquired: IP=192.168.178.30 , Gateway=192.168.178.1
TCP Echo example started
tcpHandler: Creating thread clientfd = 1
tcpWorker: start clientfd = 0x1
tcpHandler: Creating thread clientfd = 2
tcpWorker: start clientfd = 0x2
So far so good. But some seconds/ minutes later the board stops communication. The board also disappears from the list of connected devices in my AP.
There is also no serial debug output at this moment. Some minutes later I got the debug output: "tcpWorker stop clientfd" for each opened connection. The board is in a disconnected state and doesn't reconnect.
The same things happens if I ping the board. After some time the ping command tells me: "Destination Host Unreachable".
Does anybody know what could be the reason for this? The level of the Wifi signals seems to be all right.
Is there an callback which I can connect to my serial debug output?
I am new to this area so please forgive me if that is a stupid question. ;)
Many thanks,
Roman Jordan