This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1837MOD: Whether will driver and firmware be loaded to wl1837 if there is not 32.768 kHz?

Part Number: WL1837MOD
Other Parts Discussed in Thread: WL1837

Tool/software: Linux

Hello

The vibrid vf6xx processor is connected to wl1837 on our board.
We use timesys linux kernel 3.13 in our board.
On our board 32.768 kHz is not connected  to EXT_32K pin.

I so understand, driver and firmware will be loaded to wl1837
after assertion of the wlan_en signal. (Correct me if I am mistaken).

My quastion:
Whether will driver and firmware be loaded to wl1837 if there is not 32.768 kHz?

Thanks