Other Parts Discussed in Thread: CC3200, TVP5150,
Hi !
I would like to read video data from a camera outputting PAL/NTSC with my CC3200-LAUNCHXL. The CC3200 MCU features an 8-bit parallel camera interface, so I could use a PAL/NTSC to 8-bit parallel decoder like the TVP5150. However, all of the decoders I have found output 8-bit ITU-R BT.656 format. And this where I am beginning to have troubles. From the complete datasheet of the CC3200, we can read p429 that BT mode is not supported, but we can also read in the camera control register description p444 that some bits are dedicated to 8-bit parallel in BT mode (bits 12, 3-0).
So here are my questions :
Can the CC3200 MCU read 8-bit parallel in BT mode ?
If no, is there any other PAL/NTSC decoder outputting valid format for my CC3200 ?
Link to complete CC3200 datasheet : http://www.ti.com/lit/ug/swru367d/swru367d.pdf
Thank you