Part Number: WL1837MOD
Tool/software: Linux
Hello,
I have set up a mesh network. What I want to do next is make it so that every node that joins the network can connect to the internet. What are the steps I can take to accomplish this?
Currently, I have a node acting as a mesh portal (Mesh + STA modes), and it can connect to the internet. Additionally, I have a node in the mesh network acting as a mesh point (mesh standalone). However, the mesh point cannot connect to the internet (can't ping google.com or the ip), but the mesh nodes can ping each other. All roles (mesh, STA) are on channel 149/frequency 5745 MHz.
Using iw dev mesh0 station dump gives me this information:
root@am335x-evm:/usr/share/wl18xx# iw dev mesh0 station dump
Station 7c:ec:79:c8:4f:7d (on mesh0)
inactive time: 230 ms
rx bytes: 41732
rx packets: 639
tx bytes: 1639
tx packets: 16
tx retries: 0
tx failed: 0
signal: 0 dBm
signal avg: -63 dBm
Toffset: -10229304724880 us
tx bitrate: 150.0 MBit/s MCS 7 40MHz short GI
rx bitrate: 65.0 MBit/s MCS 7
expected throughput: 140.625Mbps
mesh llid: 0
mesh plid: 0
mesh plink: ESTAB
mesh local PS mode: ACTIVE
mesh peer PS mode: ACTIVE
mesh non-peer PS mode: ACTIVE
authorized: yes
authenticated: yes
preamble: long
WMM/WME: yes
MFP: no
TDLS peer: no
I am using 2 Beaglebone Black boards with E14's wireless capes.
Wlcore Firmware Versions: 8.9.0.0.79 and 8.2.0.0.242
Hostapd v2.6
Wpa_supplicant v2.6