Other Parts Discussed in Thread: STRIKE, CC31XXEMUBOOST, CC3100
Tool/software: Code Composer Studio
Hello!
I am currently working with a CC3100Boost board atop a TM4C123GH6PMXL board. Previously, I had TCP file transmissions working. After I had that working, I wanted to try to send data out of UART, and so I connected pins and tried sending data to UART3, and obviously found it conflicted with other pins.
After this, I found my previous code no longer worked - and neither did the examples provided (namely testing on the getting_started_with_wlan_station example). I have since tried reflashing the CC3100BOOST with a CC31XXXEMUBOOST, as well as reuploading the service pack.
Inspecting through Code Composer Studio's debugger mode, there are a few things that strike me as odd. Firstly, while my code seemed to go through the configureSimpleLinkToDefaultState rather quickly, it now takes a large amount of time just to get past the first sl_Start call inside of the function, and currently returns a value of (-2). Also, while I was generating an event previously when my code was working, it may be worth noting that I receive a SL_DEVICE_DRIVER_TIMEOUT_ASYNC_EVENT, with a deviceEvent of status 0, and sender of SL_ERR_SENDER_MON.
Thank you for all of your help, and have a great day