Hello,
I going to use the CC3235MODSF on a new design. However I am confused if I should be including external flash. The CC3235MODSF EVM includes external flash on the schematic.However, the module already contains 1-MB flash, which I already thought was for the purpose of storing application code, service pack files, system files, configuration files, cert files, etc.
I am unsure why does a CC3235MODSF need an external flash besides the 1-MB flash build on the module.
Is it if the code size or other files are too big?