I am attempting a socket connection to a PC from the SimpleLink Module. Everything appears ok except the sl_Connect function. It hangs when I call it. if I trace the code in sl_socket.c the hanging statement is highlighted in the attached image. Either statement hangs whether it's blocking or non-blocking. If I comment out the highlighted code the connection establishes and the rest of the socket calls seem to work fine. What am I missing? It is lines 500/506 in sl_socket.c in case the screenshot is fuzzy.
Thanks,