Part Number: CC3120BOOST
Other Parts Discussed in Thread: CC3120
Tool/software: Code Composer Studio
Hello
I'm having issue when communicating firebase real time database from CC3120 wifi module using RESTFUL API. I found that its root CA is missing from the CC3120 Simplelink root CA catalog. Firebase uses "GTS CA 101" as its root CA and it is missing in CC3120 root CA catalog. Could you please help to check whether it is still possible to communicate with firebase further? If so, could you please show a way to add the missing cert inside? Thank you.
The following link shows the simplelink root CA catalogue.
This link indicates firebase root CA. Firebase Root CA can be checked here https://www.digicert.com/help/ where https://minmin-68c89.firebaseio.com as the host to search.
Regards
Min Min