Using wpa_supplicant 2.8
If I use p2p_connect mac_address pbc go_intent=11 ht40 to establish a WiFi direct connection in response to an invitation from a Samsung Galaxy S10 mobile device, my WLl1837MOD device is the group owner and the connection is established with band 5GHz channel 36 wide channel 38 channel width 40Mhz.
If I use p2p_connect mac_address pbc go_intent=7 ht40 to establish a WiFi direct connection in response to an invitation from a Samsung Galaxy S10 mobile device, my WLl1837MOD device is the client and the connection is established with band 5GHz channel 149 wide channel 155 channel width 80Mhz.
I understand the channels in each case are based on the scan results, but what I would like to know is whether there is a way to achieve the 80Mhz connection with a different set of options in the first example (an alternative to ht40).