This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: CC3220SF-LAUNCH pad : how to use external UART ?

Expert 2065 points
Part Number: CC3220SF-LAUNCHXL


I'm trying to route CC3220 UART to that 20-pin connector, and use with external connection to PC.

Reading this launchpad guide,  per 2.5.7 I switched the jumpers, but , I cannot get anything through that connector - using the RX, TX lines.

Also, it seems the default app, pre-programmed , does not operate / start-up normally if those mentioned jumpers, are switched from Virtual COM to the 20-pin header. 

.. Why?  Any help whats missing?

  • Hi,

    This behaviour is expected in case you are using default SOP mode 0-1-0 (2-1-0). In this mode is bootlaoder mode started by state of RX line after reset. By switching to 20-pin connector is state of RX pin not defined (is at low state) and devices goes into boorloader mode.

    You have two options:

    • use SOP mode 0-0-0 for when you need to execute code
    • add weak pull-up to RX line (let say 10k to +3.3V)

    Jan

  • Hi Jan,

    Yes, thank you on the SOP, that explains it. I've found the Functional Configurations table for SOP now.

    But, still nothing comes up on the serial that I connect to those UART pins (unless they not in UART mode by default/default app .. ?).  Device , or the app verified running by it blinking leds as before, per that demo app.

    Missing something else on that UART usage ..  

    EDIT:  Aha, it goes to p55 & p57, got it.